<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kinetis 1.8 volts I/O in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-1-8-volts-I-O/m-p/323210#M14697</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The P5-9V_VIN pin is used to apply a source voltage to feed the board, this voltage enters to a 3V3 regulator to use this voltage as source of the Microcontroller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45169i8C5135BAEE558031/image-size/large?v=v2&amp;amp;px=999" title="5-9VIN.png" alt="5-9VIN.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The microcontroller can operate in two voltages range where the output voltage is defined here:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45170i2F855A73D3D4C9C8/image-size/large?v=v2&amp;amp;px=999" title="output voltage.png" alt="output voltage.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As you can see the Output voltage is VDD-0.5 of a pin in this two ranges of operation. According to this data you need to operate VDD at 2.3 V to meet 1.8 volts this when IOH = -1.5 mA. Running the microcontroller at the level 1.71 V &amp;lt;= VDD &amp;lt;= 2.7 V also make that all the input voltage coming from the module need to be at this range:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45171iAD61ACC8F0B2151E/image-size/large?v=v2&amp;amp;px=999" title="output voltage.png" alt="output voltage.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;So, I recommend to you to run the microcontroller at the high level 2.7 V &amp;lt;= VDD &amp;lt;= 3.6 V and use a level shifter to manage the this voltage issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. It would be nice!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Jul 2014 00:06:07 GMT</pubDate>
    <dc:creator>adriancano</dc:creator>
    <dc:date>2014-07-22T00:06:07Z</dc:date>
    <item>
      <title>Kinetis 1.8 volts I/O</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-1-8-volts-I-O/m-p/323209#M14696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm new to Kinetis and I need to communicate to a GSM module that runs at 1.8 volts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How am I able to configure the FRDM-KL05Z board to use some I/Os at that voltage level?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see that there is a reference to that supply voltage at the P5-9V_VIN pin but I'm not sure how to set it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anybody help me with that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd really appreciate it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jul 2014 22:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-1-8-volts-I-O/m-p/323209#M14696</guid>
      <dc:creator>luizmartins</dc:creator>
      <dc:date>2014-07-21T22:25:32Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis 1.8 volts I/O</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-1-8-volts-I-O/m-p/323210#M14697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The P5-9V_VIN pin is used to apply a source voltage to feed the board, this voltage enters to a 3V3 regulator to use this voltage as source of the Microcontroller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45169i8C5135BAEE558031/image-size/large?v=v2&amp;amp;px=999" title="5-9VIN.png" alt="5-9VIN.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The microcontroller can operate in two voltages range where the output voltage is defined here:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45170i2F855A73D3D4C9C8/image-size/large?v=v2&amp;amp;px=999" title="output voltage.png" alt="output voltage.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As you can see the Output voltage is VDD-0.5 of a pin in this two ranges of operation. According to this data you need to operate VDD at 2.3 V to meet 1.8 volts this when IOH = -1.5 mA. Running the microcontroller at the level 1.71 V &amp;lt;= VDD &amp;lt;= 2.7 V also make that all the input voltage coming from the module need to be at this range:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45171iAD61ACC8F0B2151E/image-size/large?v=v2&amp;amp;px=999" title="output voltage.png" alt="output voltage.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;So, I recommend to you to run the microcontroller at the high level 2.7 V &amp;lt;= VDD &amp;lt;= 3.6 V and use a level shifter to manage the this voltage issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. It would be nice!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jul 2014 00:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-1-8-volts-I-O/m-p/323210#M14697</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2014-07-22T00:06:07Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis 1.8 volts I/O</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-1-8-volts-I-O/m-p/323211#M14698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Adrian, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your fast answer. But, how am I able to set VDD to 2.3 V ? I mean, at each pin / connection? When I'm using the &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;FRDM-KL05Z board&lt;/SPAN&gt;, I don't see this much flexibility at the reference manual. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's not a problem to me to have all I/O to work @ 1.8 volts, actually this is good to me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jul 2014 03:01:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-1-8-volts-I-O/m-p/323211#M14698</guid>
      <dc:creator>luizmartins</dc:creator>
      <dc:date>2014-07-22T03:01:46Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis 1.8 volts I/O</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-1-8-volts-I-O/m-p/323212#M14699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you can see in the picture of the schematic in my last answer there is a 3.3 Voltage Regulator. To feed the MCU with a different voltage you can use the battery input to source a voltage that is not regulated by the NCP1117 regulator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jul 2014 14:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-1-8-volts-I-O/m-p/323212#M14699</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2014-07-22T14:59:43Z</dc:date>
    </item>
  </channel>
</rss>