<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: got error while executing CAN code</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/got-error-while-executing-CAN-code/m-p/322977#M14683</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sree venkedesh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you built the BSP for twrk20d72m firstly before compiling the flexcan example? The BSP project file is in "C:\Freescale\Freescale_MQX_4_1\build\twrk20d72m\iar" for IAR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day!&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Jul 2014 05:27:24 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2014-07-22T05:27:24Z</dc:date>
    <item>
      <title>got error while executing CAN code</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/got-error-while-executing-CAN-code/m-p/322976#M14682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Error[Li005]: no definition for "_io_printf" [referenced from C:\Freescale\Freescale_MQX_4_1\mqx\examples\can\flexcan\build\iar\flexcan_twrk20d72m\Debug\Obj\ &lt;/P&gt;&lt;P&gt;main.o] &lt;/P&gt;&lt;P&gt;Error[Li005]: no definition for "_task_block" [referenced from C:\Freescale\Freescale_MQX_4_1\mqx\examples\can\flexcan\build\iar\flexcan_twrk20d72m\Debug\ &lt;/P&gt;&lt;P&gt;Obj\main.o] &lt;/P&gt;&lt;P&gt;Error[Li005]: no definition for "_bsp_get_flexcan_base_address" [referenced from C:\Freescale\Freescale_MQX_4_1\mqx\examples\can\flexcan\build\iar\ &lt;/P&gt;&lt;P&gt;flexcan_twrk20d72m\Debug\Obj\main.o] &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jul 2014 12:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/got-error-while-executing-CAN-code/m-p/322976#M14682</guid>
      <dc:creator>sreevenkedesh</dc:creator>
      <dc:date>2014-07-21T12:03:50Z</dc:date>
    </item>
    <item>
      <title>Re: got error while executing CAN code</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/got-error-while-executing-CAN-code/m-p/322977#M14683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sree venkedesh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you built the BSP for twrk20d72m firstly before compiling the flexcan example? The BSP project file is in "C:\Freescale\Freescale_MQX_4_1\build\twrk20d72m\iar" for IAR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day!&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jul 2014 05:27:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/got-error-while-executing-CAN-code/m-p/322977#M14683</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-07-22T05:27:24Z</dc:date>
    </item>
    <item>
      <title>Re: got error while executing CAN code</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/got-error-while-executing-CAN-code/m-p/322978#M14684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sree venkedesh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How about this issue on your side? Actually I can compile it correctly after the whole BSP is built. Please note you have to batch build the whole libs before compiling any MQX example. Please refer to the following for more details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45182iE535ACCECE5DFA6F/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45183i527B87AFB3597C7A/image-size/large?v=v2&amp;amp;px=999" title="1-1.png" alt="1-1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45184i707E3BCDF4F85996/image-size/large?v=v2&amp;amp;px=999" title="2.png" alt="2.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;B.R&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jul 2014 05:37:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/got-error-while-executing-CAN-code/m-p/322978#M14684</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-07-23T05:37:58Z</dc:date>
    </item>
  </channel>
</rss>