<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックI'm using lptmr delay in KL46 controller. I was able to provide the minimum delay in 1millisecond for instruction. I require the delay in microsecond or possibly in nanoseconds.  Can anyone suggest me the feasibility for the same in KL46 controller ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-using-lptmr-delay-in-KL46-controller-I-was-able-to-provide/m-p/322578#M14630</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using lptmr delay in KL46 controller. I was able to provide the minimum delay in 1millisecond for instruction. I require the delay in microsecond or possibly in nanoseconds.&amp;nbsp; Can anyone suggest me the feasibility for the same in KL46 controller ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Jun 2014 14:14:24 GMT</pubDate>
    <dc:creator>yusupkhan</dc:creator>
    <dc:date>2014-06-21T14:14:24Z</dc:date>
    <item>
      <title>I'm using lptmr delay in KL46 controller. I was able to provide the minimum delay in 1millisecond for instruction. I require the delay in microsecond or possibly in nanoseconds.  Can anyone suggest me the feasibility for the same in KL46 controller ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-using-lptmr-delay-in-KL46-controller-I-was-able-to-provide/m-p/322578#M14630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using lptmr delay in KL46 controller. I was able to provide the minimum delay in 1millisecond for instruction. I require the delay in microsecond or possibly in nanoseconds.&amp;nbsp; Can anyone suggest me the feasibility for the same in KL46 controller ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jun 2014 14:14:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-using-lptmr-delay-in-KL46-controller-I-was-able-to-provide/m-p/322578#M14630</guid>
      <dc:creator>yusupkhan</dc:creator>
      <dc:date>2014-06-21T14:14:24Z</dc:date>
    </item>
    <item>
      <title>Re: I'm using lptmr delay in KL46 controller. I was able to provide the minimum delay in 1millisecond for instruction. I require the delay in microsecond or possibly in nanoseconds.  Can anyone suggest me the feasibility for the same in KL46 controller ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-using-lptmr-delay-in-KL46-controller-I-was-able-to-provide/m-p/322579#M14631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can select the source of the LPTMR clock.&lt;/P&gt;&lt;P&gt;If you have an 8MHz oscillator connected and use this as source you will have 125ns timer resolution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jun 2014 15:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-m-using-lptmr-delay-in-KL46-controller-I-was-able-to-provide/m-p/322579#M14631</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-06-21T15:16:51Z</dc:date>
    </item>
  </channel>
</rss>