<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Do Kinetis K22 has internal pullups on the SDHC peripheral lines?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-Kinetis-K22-has-internal-pullups-on-the-SDHC-peripheral-lines/m-p/322257#M14545</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pasquale&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can decide whether pull-ups are enabled or not when configuring each pin. See PORTn_PCRx register.&lt;/P&gt;&lt;P&gt;The pull-up resistors will have a wider tolerance spread than external ones though.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Jul 2014 15:59:43 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-07-18T15:59:43Z</dc:date>
    <item>
      <title>Do Kinetis K22 has internal pullups on the SDHC peripheral lines?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-Kinetis-K22-has-internal-pullups-on-the-SDHC-peripheral-lines/m-p/322256#M14544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Or i need to put them external?&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;Pasquale&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jul 2014 15:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-Kinetis-K22-has-internal-pullups-on-the-SDHC-peripheral-lines/m-p/322256#M14544</guid>
      <dc:creator>pasqualelongo</dc:creator>
      <dc:date>2014-07-18T15:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: Do Kinetis K22 has internal pullups on the SDHC peripheral lines?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-Kinetis-K22-has-internal-pullups-on-the-SDHC-peripheral-lines/m-p/322257#M14545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pasquale&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can decide whether pull-ups are enabled or not when configuring each pin. See PORTn_PCRx register.&lt;/P&gt;&lt;P&gt;The pull-up resistors will have a wider tolerance spread than external ones though.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jul 2014 15:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-Kinetis-K22-has-internal-pullups-on-the-SDHC-peripheral-lines/m-p/322257#M14545</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-07-18T15:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: Do Kinetis K22 has internal pullups on the SDHC peripheral lines?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-Kinetis-K22-has-internal-pullups-on-the-SDHC-peripheral-lines/m-p/322258#M14546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Longo&lt;/P&gt;&lt;P&gt;I agree with Mark. It is better to add external pull-up resistor. The internal resistor is a weak pull-up. So you need add a strong pull-up external to ensure communication is good on no good layout condition. Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jul 2014 06:43:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-Kinetis-K22-has-internal-pullups-on-the-SDHC-peripheral-lines/m-p/322258#M14546</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2014-07-21T06:43:37Z</dc:date>
    </item>
    <item>
      <title>Re: Do Kinetis K22 has internal pullups on the SDHC peripheral lines?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-Kinetis-K22-has-internal-pullups-on-the-SDHC-peripheral-lines/m-p/322259#M14547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Mark and Paul,&lt;/P&gt;&lt;P&gt;I'll perform some tests using internal pullups, if i'll found problems i'll install external.&lt;/P&gt;&lt;P&gt;Will keep you updated&lt;/P&gt;&lt;P&gt;Pasquale&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jul 2014 07:22:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-Kinetis-K22-has-internal-pullups-on-the-SDHC-peripheral-lines/m-p/322259#M14547</guid>
      <dc:creator>pasqualelongo</dc:creator>
      <dc:date>2014-07-21T07:22:05Z</dc:date>
    </item>
  </channel>
</rss>