<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Initial support for low-power in Linux on Kinetis</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Initial-support-for-low-power-in-Linux-on-Kinetis/m-p/322043#M14502</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Emcraft has made available an initial implementation of low-power mode in Linux on the Kinetis K70 &amp;amp; K61 processors. Using the Linux "suspend-to-RAM" framework, the power consumption of the Kinetis running Linux (using the Emcraft System-On-Module as the hardware platform) goes down to as low as 600-700 uA while in suspend. Wake-up is instantenous on configured I/O events such as RTC alarm triggers or activity on UART RX. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Details available from: &lt;A href="http://www.emcraft.com/som/k70/linux-low-power-mode-on-kinetis" title="http://www.emcraft.com/som/k70/linux-low-power-mode-on-kinetis"&gt;Linux Low-Power Mode on Kinetis&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Jun 2014 08:35:38 GMT</pubDate>
    <dc:creator>vladimirkhusain</dc:creator>
    <dc:date>2014-06-20T08:35:38Z</dc:date>
    <item>
      <title>Initial support for low-power in Linux on Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Initial-support-for-low-power-in-Linux-on-Kinetis/m-p/322043#M14502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Emcraft has made available an initial implementation of low-power mode in Linux on the Kinetis K70 &amp;amp; K61 processors. Using the Linux "suspend-to-RAM" framework, the power consumption of the Kinetis running Linux (using the Emcraft System-On-Module as the hardware platform) goes down to as low as 600-700 uA while in suspend. Wake-up is instantenous on configured I/O events such as RTC alarm triggers or activity on UART RX. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Details available from: &lt;A href="http://www.emcraft.com/som/k70/linux-low-power-mode-on-kinetis" title="http://www.emcraft.com/som/k70/linux-low-power-mode-on-kinetis"&gt;Linux Low-Power Mode on Kinetis&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jun 2014 08:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Initial-support-for-low-power-in-Linux-on-Kinetis/m-p/322043#M14502</guid>
      <dc:creator>vladimirkhusain</dc:creator>
      <dc:date>2014-06-20T08:35:38Z</dc:date>
    </item>
  </channel>
</rss>