<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can FlexCAN work at No-interrupt mode? The example when CAN receive data there will be a interrupt, the ISR read it, I don't want use this way. I want read the data when I want. in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-FlexCAN-work-at-No-interrupt-mode-The-example-when-CAN/m-p/321862#M14482</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My MCU is K64, how to set the register?&lt;/P&gt;&lt;P&gt;And after I disable the interrupt, when I read CAN RX mailbox, there was a error, so FlexCAN only can work at interrups mode?&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BRs&lt;/P&gt;&lt;P&gt;Li&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Jun 2014 03:40:26 GMT</pubDate>
    <dc:creator>jieli</dc:creator>
    <dc:date>2014-06-20T03:40:26Z</dc:date>
    <item>
      <title>Can FlexCAN work at No-interrupt mode? The example when CAN receive data there will be a interrupt, the ISR read it, I don't want use this way. I want read the data when I want.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-FlexCAN-work-at-No-interrupt-mode-The-example-when-CAN/m-p/321862#M14482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My MCU is K64, how to set the register?&lt;/P&gt;&lt;P&gt;And after I disable the interrupt, when I read CAN RX mailbox, there was a error, so FlexCAN only can work at interrups mode?&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BRs&lt;/P&gt;&lt;P&gt;Li&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jun 2014 03:40:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-FlexCAN-work-at-No-interrupt-mode-The-example-when-CAN/m-p/321862#M14482</guid>
      <dc:creator>jieli</dc:creator>
      <dc:date>2014-06-20T03:40:26Z</dc:date>
    </item>
    <item>
      <title>Re: Can FlexCAN work at No-interrupt mode? The example when CAN receive data there will be a interrupt, the ISR read it, I don't want use this way. I want read the data when I want.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-FlexCAN-work-at-No-interrupt-mode-The-example-when-CAN/m-p/321863#M14483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jie:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well if you are using interruption configuration you will certainly have to read data when interruption rises, but if you do not want to use this scheme consider polling.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Perla Moncada&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jun 2014 17:27:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-FlexCAN-work-at-No-interrupt-mode-The-example-when-CAN/m-p/321863#M14483</guid>
      <dc:creator>perlam_i_au</dc:creator>
      <dc:date>2014-06-20T17:27:26Z</dc:date>
    </item>
    <item>
      <title>Re: Can FlexCAN work at No-interrupt mode? The example when CAN receive data there will be a interrupt, the ISR read it, I don't want use this way. I want read the data when I want.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-FlexCAN-work-at-No-interrupt-mode-The-example-when-CAN/m-p/321864#M14484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Moncada&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I don't want to use interrupt, but after I disable interrupt, there was error when I read data from CAN, So I though there maybe some registers that I should set to polling mode.&lt;/P&gt;&lt;P&gt;Is there such register?&lt;/P&gt;&lt;P&gt;Another question, I want the new data overwrite the old one automatically, is it available?&lt;/P&gt;&lt;P&gt;thank you for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BRs,&lt;/P&gt;&lt;P&gt;Jie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jun 2014 01:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-FlexCAN-work-at-No-interrupt-mode-The-example-when-CAN/m-p/321864#M14484</guid>
      <dc:creator>jieli</dc:creator>
      <dc:date>2014-06-23T01:41:59Z</dc:date>
    </item>
    <item>
      <title>Re: Can FlexCAN work at No-interrupt mode? The example when CAN receive data there will be a interrupt, the ISR read it, I don't want use this way. I want read the data when I want.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-FlexCAN-work-at-No-interrupt-mode-The-example-when-CAN/m-p/321865#M14485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend to use CodeWarrior with embedded Processor Expert software, which provides CAN_LDD component.&lt;/P&gt;&lt;P&gt;In the typical usage CAN_LDD provides interrupt mode and polling mode application demo.&lt;/P&gt;&lt;P&gt;More detailed info, please check CAN_LDD help file.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45063iF1BC6E234BBE3A36/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Wish it helps.&lt;BR /&gt;best regards &lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 08:27:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-FlexCAN-work-at-No-interrupt-mode-The-example-when-CAN/m-p/321865#M14485</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-07-16T08:27:35Z</dc:date>
    </item>
  </channel>
</rss>