<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKE06 48MHz operation</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-48MHz-operation/m-p/320950#M14377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think I already know the answer to this, but it seems that in order to get 48 MHz operation from an external crystal, it is necessary to use a 9.6 MHz crystal, a 19.2 MHz crystal, or an external 48 MHz oscillator, is this correct?&amp;nbsp; It doesn't appear that this is possible using an 8 MHz or 16 MHz crystal, which are readily available.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jun 2014 17:24:14 GMT</pubDate>
    <dc:creator>davidsherman</dc:creator>
    <dc:date>2014-06-18T17:24:14Z</dc:date>
    <item>
      <title>KE06 48MHz operation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-48MHz-operation/m-p/320950#M14377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think I already know the answer to this, but it seems that in order to get 48 MHz operation from an external crystal, it is necessary to use a 9.6 MHz crystal, a 19.2 MHz crystal, or an external 48 MHz oscillator, is this correct?&amp;nbsp; It doesn't appear that this is possible using an 8 MHz or 16 MHz crystal, which are readily available.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jun 2014 17:24:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-48MHz-operation/m-p/320950#M14377</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2014-06-18T17:24:14Z</dc:date>
    </item>
    <item>
      <title>Re: KE06 48MHz operation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-48MHz-operation/m-p/320951#M14378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you are correct, the FLL reference clock divider and the fixed 1280 multiplication factor will not allow you to use 8 MHz or 16 MHz crystal. An alternative would be to use FEI mode and trimming the internal reference clock to 37500 Hz.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jun 2014 02:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-48MHz-operation/m-p/320951#M14378</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-06-19T02:09:24Z</dc:date>
    </item>
    <item>
      <title>Re: KE06 48MHz operation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-48MHz-operation/m-p/320952#M14379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jorge, I think that seems to be the case.&amp;nbsp; I don't think the internal oscillator will be stable enough for the application I'm intending.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jun 2014 12:33:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-48MHz-operation/m-p/320952#M14379</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2014-06-20T12:33:47Z</dc:date>
    </item>
  </channel>
</rss>