<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: GPIO HI-Impedance configuration and pullup/pulldown in MK20DX series ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-HI-Impedance-configuration-and-pullup-pulldown-in-MK20DX/m-p/320879#M14376</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I freely acknowledge that pulling a 'full picture' of functions from these 1000+ page documents can be daunting.&amp;nbsp; In particular, these Freescale Kinetis manuals suffer from a confusion in that the 'peripheral function' descriptions are 'generic' per the design of that silicon module, but many times you have to correlate info from Chapter 3 (and other places!)&amp;nbsp; to understand what clocks/options/shortcomings come with a particular 'chip'.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additionally, they DON'T document any details that are considered 'ARM core', leaving THAT to be culled from &lt;A href="http://www.arm.com/"&gt;www.arm.com&lt;/A&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Jul 2014 13:03:26 GMT</pubDate>
    <dc:creator>egoodii</dc:creator>
    <dc:date>2014-07-16T13:03:26Z</dc:date>
    <item>
      <title>GPIO HI-Impedance configuration and pullup/pulldown in MK20DX series ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-HI-Impedance-configuration-and-pullup-pulldown-in-MK20DX/m-p/320876#M14373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sirs,&lt;/P&gt;&lt;P&gt;I have few questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Does anyone knows if there's the possibility to configure the GPIO pins on K20 Sub-family microcontrollers MK20DX64VLH7, MK20DX128VLH7, MK20DX256VLH7 to put them in HI-Z status?&lt;/LI&gt;&lt;LI&gt;The GPIO's do have a pullup or a pulldown? In what GPIO conditions?&lt;/LI&gt;&lt;LI&gt;Are there different strengths for the GPIOs current capability? Are the strengths configurable, or there are differences from pin to pin?&lt;/LI&gt;&lt;LI&gt;In reset condition, or start-up condition, what is the GPIO status, in term of direction, pullup configuration, output status?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could not find that information on the documents I've read, that are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K20P64M72SF1&lt;/P&gt;&lt;P&gt;Rev. 3, 11/2012&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K20P64M72SF1RM&lt;/P&gt;&lt;P&gt;Rev. 1.1, Dec 2012&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I need any other document?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you everybody.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michele Canepa, Electrical Engineer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 10:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-HI-Impedance-configuration-and-pullup-pulldown-in-MK20DX/m-p/320876#M14373</guid>
      <dc:creator>michelecanepa</dc:creator>
      <dc:date>2014-07-16T10:34:24Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO HI-Impedance configuration and pullup/pulldown in MK20DX series ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-HI-Impedance-configuration-and-pullup-pulldown-in-MK20DX/m-p/320877#M14374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Referencing:&lt;/P&gt;&lt;P&gt;K20P64M72SF1RM&lt;/P&gt;&lt;P&gt;Rev. 1.1, Dec 2012&lt;/P&gt;&lt;P&gt;1 - All GPIO are 'Hi-Z' when configured as inputs -- see 49.2.6.&lt;/P&gt;&lt;P&gt;2 - Most GPIO pins have the options under 'PORT control' 11.14.1, the pull-enable and up/down being the two LSBs.&lt;/P&gt;&lt;P&gt;3 - See above -- also a function of PORT control.&lt;/P&gt;&lt;P&gt;4 - All GPIO pins will be 'input' (Hi-Z) as per the 'reset condition' outlined in 49.2.6.&amp;nbsp; However, for a complete definition of 'pin state at reset' refer to chapter 10.&amp;nbsp; 10.2.2 lists some 'special' reset-values for some members of Port A PORT control, but more particularly the table in 10.3.1 lists the 'default' operational-mode for every pin on the package.&amp;nbsp; Most pins default to their 'analog' function -- Alternate '0' --&amp;nbsp; (except the debug pins, on Port A, as selected by those 'special' PORT control values), as this has the least restriction on external connections.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 12:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-HI-Impedance-configuration-and-pullup-pulldown-in-MK20DX/m-p/320877#M14374</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2014-07-16T12:29:06Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO HI-Impedance configuration and pullup/pulldown in MK20DX series ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-HI-Impedance-configuration-and-pullup-pulldown-in-MK20DX/m-p/320878#M14375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much Earl !&lt;/P&gt;&lt;P&gt;The answers to all my questions are definitely in that document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Michele&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 12:55:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-HI-Impedance-configuration-and-pullup-pulldown-in-MK20DX/m-p/320878#M14375</guid>
      <dc:creator>michelecanepa</dc:creator>
      <dc:date>2014-07-16T12:55:20Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO HI-Impedance configuration and pullup/pulldown in MK20DX series ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-HI-Impedance-configuration-and-pullup-pulldown-in-MK20DX/m-p/320879#M14376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I freely acknowledge that pulling a 'full picture' of functions from these 1000+ page documents can be daunting.&amp;nbsp; In particular, these Freescale Kinetis manuals suffer from a confusion in that the 'peripheral function' descriptions are 'generic' per the design of that silicon module, but many times you have to correlate info from Chapter 3 (and other places!)&amp;nbsp; to understand what clocks/options/shortcomings come with a particular 'chip'.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additionally, they DON'T document any details that are considered 'ARM core', leaving THAT to be culled from &lt;A href="http://www.arm.com/"&gt;www.arm.com&lt;/A&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 13:03:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-HI-Impedance-configuration-and-pullup-pulldown-in-MK20DX/m-p/320879#M14376</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2014-07-16T13:03:26Z</dc:date>
    </item>
  </channel>
</rss>