<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K70 ADC hardware average function in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-ADC-hardware-average-function/m-p/320825#M14370</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the K70 Reference Manual, under section 39, 16-bit ADC it has been mentioned that hardware average function is supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the K70 Datasheet document, (Doc. Name: K70P256M120SF3) under table -29 it is mentioned that no ADC hardware averaging function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the hardware averaging function present as part of 16-bit ADC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Hemanth&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: 10pt;"&gt;&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: 10pt;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jun 2014 10:22:25 GMT</pubDate>
    <dc:creator>hemanthkumarven</dc:creator>
    <dc:date>2014-06-18T10:22:25Z</dc:date>
    <item>
      <title>K70 ADC hardware average function</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-ADC-hardware-average-function/m-p/320825#M14370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the K70 Reference Manual, under section 39, 16-bit ADC it has been mentioned that hardware average function is supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the K70 Datasheet document, (Doc. Name: K70P256M120SF3) under table -29 it is mentioned that no ADC hardware averaging function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the hardware averaging function present as part of 16-bit ADC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Hemanth&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: 10pt;"&gt;&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: 10pt;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jun 2014 10:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-ADC-hardware-average-function/m-p/320825#M14370</guid>
      <dc:creator>hemanthkumarven</dc:creator>
      <dc:date>2014-06-18T10:22:25Z</dc:date>
    </item>
    <item>
      <title>Re: K70 ADC hardware average function</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-ADC-hardware-average-function/m-p/320826#M14371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, hardware averaging is supported by ADC in K70. I think you refer to the next part of the datasheet right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43271iCF6F3CE7DEEC6306/image-size/large?v=v2&amp;amp;px=999" title="ADC.png" alt="ADC.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The "No ADC hardware averaging" just represents a condition. It means that a Crate between 37.037 and 461.467 Ksps can be achieved using continuous conversions and *without* enabling hardware averaging, but it does not mean that averaging is not supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this clarifies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!,&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jun 2014 13:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-ADC-hardware-average-function/m-p/320826#M14371</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-06-18T13:19:37Z</dc:date>
    </item>
    <item>
      <title>Re: K70 ADC hardware average function</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-ADC-hardware-average-function/m-p/320827#M14372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the Quick Reply Jorge..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Really appreciated..&lt;/P&gt;&lt;P&gt;Hemanth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jun 2014 13:26:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-ADC-hardware-average-function/m-p/320827#M14372</guid>
      <dc:creator>hemanthkumarven</dc:creator>
      <dc:date>2014-06-18T13:26:49Z</dc:date>
    </item>
  </channel>
</rss>