<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Help me with uart0 dma in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-me-with-uart0-dma/m-p/320325#M14342</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KL25 CW UART TX DMA is supported in the uTasker project : &lt;A href="http://www.utasker.com/forum/index.php?topic=1721.0" title="http://www.utasker.com/forum/index.php?topic=1721.0"&gt;http://www.utasker.com/forum/index.php?topic=1721.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;However DMA at the receiver is not included since the KL DMA doesn't support free-runnning circular buffers - that is, it is not as useful as the DMA controller in the K devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Jul 2014 12:53:04 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-07-15T12:53:04Z</dc:date>
    <item>
      <title>Help me with uart0 dma</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-me-with-uart0-dma/m-p/320324#M14341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help me how to implement dma on uart0 for rx and tx ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;p.s. I'm using kl25 mcu and CodeWarrior as IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jul 2014 08:21:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-me-with-uart0-dma/m-p/320324#M14341</guid>
      <dc:creator>arbnorzeqiri</dc:creator>
      <dc:date>2014-07-15T08:21:57Z</dc:date>
    </item>
    <item>
      <title>Re: Help me with uart0 dma</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-me-with-uart0-dma/m-p/320325#M14342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KL25 CW UART TX DMA is supported in the uTasker project : &lt;A href="http://www.utasker.com/forum/index.php?topic=1721.0" title="http://www.utasker.com/forum/index.php?topic=1721.0"&gt;http://www.utasker.com/forum/index.php?topic=1721.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;However DMA at the receiver is not included since the KL DMA doesn't support free-runnning circular buffers - that is, it is not as useful as the DMA controller in the K devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jul 2014 12:53:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-me-with-uart0-dma/m-p/320325#M14342</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-07-15T12:53:04Z</dc:date>
    </item>
  </channel>
</rss>