<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: K60D100M unused ethernet pins</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60D100M-unused-ethernet-pins/m-p/320215#M14333</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you so much for your help! I will proceed with the design based on your help, and let you guys know how the project turns out! Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Jul 2014 14:09:20 GMT</pubDate>
    <dc:creator>zachquinn</dc:creator>
    <dc:date>2014-07-16T14:09:20Z</dc:date>
    <item>
      <title>K60D100M unused ethernet pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60D100M-unused-ethernet-pins/m-p/320213#M14331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the TWR-K60D100M and TWR-SER schematic as a guideline for moving our system to a dedicated PCB. However, I am confused by looking at page 8 of the electrical schematic for the TWR-K60D100M: Many of the pins from A12-A20 and B12-B20 do not make it back to the MCU. Most interestingly, TXCLK and RXCLK don't get bussed back...this seems like it will not function. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have some insight for this? Sorry if this is a really obvious question. I am new to the PCB field, Ethernet, and the Tower System! Any help is very appreciated. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jul 2014 21:25:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60D100M-unused-ethernet-pins/m-p/320213#M14331</guid>
      <dc:creator>zachquinn</dc:creator>
      <dc:date>2014-07-14T21:25:27Z</dc:date>
    </item>
    <item>
      <title>Re: K60D100M unused ethernet pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60D100M-unused-ethernet-pins/m-p/320214#M14332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Zac,&lt;/P&gt;&lt;P&gt;The short story is the TWR-SER card is being setup for RMII mode which reduces the number of Ethernet signals required.&lt;/P&gt;&lt;P&gt;The TWR-SER card is also sourcing the 50MHz clock to the PHY and it gets jumpered to return to the MCU/TWR-K60D100M card.&amp;nbsp; The MQX RTOS software configured to use external 50MHz clock signal as the MCU clock source.&lt;/P&gt;&lt;P&gt;With both the MCU and PHY being clocked by the same source, the clock domains are the same and the TXCLK and RXCLK are not needed.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jul 2014 21:51:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60D100M-unused-ethernet-pins/m-p/320214#M14332</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2014-07-14T21:51:00Z</dc:date>
    </item>
    <item>
      <title>Re: K60D100M unused ethernet pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60D100M-unused-ethernet-pins/m-p/320215#M14333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you so much for your help! I will proceed with the design based on your help, and let you guys know how the project turns out! Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 14:09:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60D100M-unused-ethernet-pins/m-p/320215#M14333</guid>
      <dc:creator>zachquinn</dc:creator>
      <dc:date>2014-07-16T14:09:20Z</dc:date>
    </item>
  </channel>
</rss>