<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: USB hardware design Query</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-hardware-design-Query/m-p/320007#M14307</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dragos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Capacitor is there. I did not understand your point regarding software issue. Could you please elaborate more on this?I am using library component for USB CDC device. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Jun 2014 06:05:34 GMT</pubDate>
    <dc:creator>Embionics</dc:creator>
    <dc:date>2014-06-21T06:05:34Z</dc:date>
    <item>
      <title>USB hardware design Query</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-hardware-design-Query/m-p/320004#M14304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with KL25Z64VFM4 controller for USB as a CDC device.&lt;/P&gt;&lt;P&gt;I have attached snap shot of USB schematic.&lt;/P&gt;&lt;P&gt;I have given external 3.3V from J4 connector as in the schematic.&lt;/P&gt;&lt;P&gt;And connected USB for testing as a CDC device.&lt;/P&gt;&lt;P&gt;It was working very well.&lt;/P&gt;&lt;P&gt;But when i am testing again i got the message from USB port that "Device is consuming more current".&lt;/P&gt;&lt;P&gt;After that i got that USB_5V and ground signal are short.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Is the attached schematic is OK for USB or do i need to make any changes in it?&lt;/P&gt;&lt;P&gt;2) Can I connect multilink for debugging when i am giving external 3.3V and USB is also connected?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Amreen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jun 2014 05:47:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-hardware-design-Query/m-p/320004#M14304</guid>
      <dc:creator>Embionics</dc:creator>
      <dc:date>2014-06-17T05:47:33Z</dc:date>
    </item>
    <item>
      <title>Re: USB hardware design Query</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-hardware-design-Query/m-p/320005#M14305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;UL&gt;&lt;LI&gt;I did not find any obvious problem in your schematic regarding the power rails however that does not rule out the possibility of a hardware failure.&lt;/LI&gt;&lt;LI&gt;Yes you can connect a debugging probe even though you supply the mcu with 3.3V VDD &lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jun 2014 18:11:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-hardware-design-Query/m-p/320005#M14305</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2014-06-17T18:11:53Z</dc:date>
    </item>
    <item>
      <title>Re: USB hardware design Query</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-hardware-design-Query/m-p/320006#M14306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Put a capacitor of at least 1uF between USB_5V and ground.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It could also be a software issue, check that you are reporting the "correct" amount of current drawn.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jun 2014 19:18:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-hardware-design-Query/m-p/320006#M14306</guid>
      <dc:creator>galadragos</dc:creator>
      <dc:date>2014-06-17T19:18:17Z</dc:date>
    </item>
    <item>
      <title>Re: USB hardware design Query</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-hardware-design-Query/m-p/320007#M14307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dragos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Capacitor is there. I did not understand your point regarding software issue. Could you please elaborate more on this?I am using library component for USB CDC device. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jun 2014 06:05:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-hardware-design-Query/m-p/320007#M14307</guid>
      <dc:creator>Embionics</dc:creator>
      <dc:date>2014-06-21T06:05:34Z</dc:date>
    </item>
    <item>
      <title>Re: USB hardware design Query</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-hardware-design-Query/m-p/320008#M14308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;THe USB descriptors have a way of "setting" the amount of current the host should give to the slave device. Historically this field would have two values that represented 100mA and 500mA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, newer USB controllers can detect the amount of current the slave is consuming and will go into current protection mode if it tries to pull too much current.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, some drivers instinctively disable the USB port power for devices that request more than 500mA of current, in their headers, because that is what the maximum amount of current a slave device should draw from the USB port.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jul 2014 18:40:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-hardware-design-Query/m-p/320008#M14308</guid>
      <dc:creator>galadragos</dc:creator>
      <dc:date>2014-07-03T18:40:57Z</dc:date>
    </item>
  </channel>
</rss>