<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Problem regarding External RTC crystal</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-regarding-External-RTC-crystal/m-p/319401#M14213</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have connected a 32Khz crystal(Abracon's ABS25-32.000KHZ-T) to be used as RTC clock input between PTC1 and PTE0. We have made such an arrangement in 40 different boards. Now we got a problem that crystal frequency is not coming. Might it be a problem with the crystal? Suggest me if there are any settings i need to do with the microcontroller when using crystal at PTC1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Embionics Technologies&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 12 Jul 2014 13:50:53 GMT</pubDate>
    <dc:creator>Embionics</dc:creator>
    <dc:date>2014-07-12T13:50:53Z</dc:date>
    <item>
      <title>Problem regarding External RTC crystal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-regarding-External-RTC-crystal/m-p/319401#M14213</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have connected a 32Khz crystal(Abracon's ABS25-32.000KHZ-T) to be used as RTC clock input between PTC1 and PTE0. We have made such an arrangement in 40 different boards. Now we got a problem that crystal frequency is not coming. Might it be a problem with the crystal? Suggest me if there are any settings i need to do with the microcontroller when using crystal at PTC1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Embionics Technologies&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Jul 2014 13:50:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-regarding-External-RTC-crystal/m-p/319401#M14213</guid>
      <dc:creator>Embionics</dc:creator>
      <dc:date>2014-07-12T13:50:53Z</dc:date>
    </item>
    <item>
      <title>Re: Problem regarding External RTC crystal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-regarding-External-RTC-crystal/m-p/319402#M14214</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am "guessing" you are using a KL25 (or similar).&lt;/P&gt;&lt;P&gt;If this is the case see &lt;A href="https://community.nxp.com/message/398099"&gt;Re: RTC_CLKIN and RTC_CLKOUT pins assignment on Kinetis&lt;/A&gt; and &lt;A href="https://community.nxp.com/message/332226"&gt;Re: KL25 RTC OSCILLATOR SELECTION&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately you can't use a crystal with this device since it doesn't have an oscillator - you would need to modify the boards and add a crystal oscillaor circuit in place fo the crystal (see the TWR-KL25Z48M circuit as reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Jul 2014 19:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-regarding-External-RTC-crystal/m-p/319402#M14214</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-07-12T19:53:21Z</dc:date>
    </item>
  </channel>
</rss>