<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Error when adding ADC component (KDS, Processor Expert) in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Error-when-adding-ADC-component-KDS-Processor-Expert/m-p/318677#M14146</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Interesting note. When you look at the Console display you still see the error even if there is not an error. I did have an error fixed it and the project now works. However, there is still an error message in the console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Type specification was not found "typeFHCS12RVAEnableRVA" symbol: RVAEnableRVA&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Type specification was not found "typeFHCS12RVAEnableRVA" symbol: RVAEnableRVA&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Error: Unknown type info: typeFHCS12RVAEnableRVA in item "Enable RVA"/RVAEnableRVA from component AD0edwb0/ADC&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Error: Unknown type info: typeFHCS12RVAEnableRVA in item "Enable RVA"/RVAEnableRVA from component AD1edwb1/ADC&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;EDWB: Mar 24, 2015 5:30:30 PM Code generation started.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;EDWB: Code generation time was 24694 ms.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;EDWB: project was successfully generated.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49562iCB0A191C3FDB592C/image-size/large?v=v2&amp;amp;px=999" title="Screen Shot 03-24-15 at 05.36 PM.PNG" alt="Screen Shot 03-24-15 at 05.36 PM.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Mar 2015 21:39:29 GMT</pubDate>
    <dc:creator>barbercolman</dc:creator>
    <dc:date>2015-03-24T21:39:29Z</dc:date>
    <item>
      <title>Error when adding ADC component (KDS, Processor Expert)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Error-when-adding-ADC-component-KDS-Processor-Expert/m-p/318675#M14144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've been able to successfully add an ADC component to my Kinetis Design Studio project using Processor Expert in the past; however, I am now not able to do so.&amp;nbsp; I receive the following messages in the console:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Error: Unknown type info: typeFHCS12RVAEnableRVA in item "Enable RVA"/RVAEnableRVA from component AD1/ADC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Type specification was not found "typeFHCS12RVAEnableRVA" symbol: RVAEnableRVA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The AdcLdd component clock settings are also not initialized as they should (or at least did in the past).&amp;nbsp; I've attached some screen captures to illustrate the symptom.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've already tried reinstalling KDS on my primary workstation as well as performing a fresh install on a different machine, but have the same results.&amp;nbsp; The only workaround I current have is to create a component template from the ADC I have successfully added to my previous project and use that, but like I said, it's a workaround and I'd like to have this working properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone had a problem like this or know what might be causing it?&amp;nbsp; It seems like the incorrect CPU is being referenced or something; though as you can see I've got the MK50FN1M0VLQ12 selected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Best Regards,&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44942i85B83B8B4EB2FC3F/image-size/large?v=v2&amp;amp;px=999" title="Capture.JPG.jpg" alt="Capture.JPG.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44943i6B61BD1EB02AB030/image-size/large?v=v2&amp;amp;px=999" title="Capture2.JPG.jpg" alt="Capture2.JPG.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44944i6B583F1ED929E0D1/image-size/large?v=v2&amp;amp;px=999" title="Capture3.JPG.jpg" alt="Capture3.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2014 21:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Error-when-adding-ADC-component-KDS-Processor-Expert/m-p/318675#M14144</guid>
      <dc:creator>acurtis</dc:creator>
      <dc:date>2014-07-10T21:15:15Z</dc:date>
    </item>
    <item>
      <title>Re: Error when adding ADC component (KDS, Processor Expert)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Error-when-adding-ADC-component-KDS-Processor-Expert/m-p/318676#M14145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The errors should disappear after you configure the timing in the ADC component. Please check that and post what is shown in Problems view if the problem persists.&lt;/P&gt;&lt;P&gt;The Console view might sometimes contain messages that do not mean an error. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jul 2014 13:17:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Error-when-adding-ADC-component-KDS-Processor-Expert/m-p/318676#M14145</guid>
      <dc:creator>Petr_H</dc:creator>
      <dc:date>2014-07-14T13:17:11Z</dc:date>
    </item>
    <item>
      <title>Re: Error when adding ADC component (KDS, Processor Expert)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Error-when-adding-ADC-component-KDS-Processor-Expert/m-p/318677#M14146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Interesting note. When you look at the Console display you still see the error even if there is not an error. I did have an error fixed it and the project now works. However, there is still an error message in the console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Type specification was not found "typeFHCS12RVAEnableRVA" symbol: RVAEnableRVA&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Type specification was not found "typeFHCS12RVAEnableRVA" symbol: RVAEnableRVA&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Error: Unknown type info: typeFHCS12RVAEnableRVA in item "Enable RVA"/RVAEnableRVA from component AD0edwb0/ADC&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Error: Unknown type info: typeFHCS12RVAEnableRVA in item "Enable RVA"/RVAEnableRVA from component AD1edwb1/ADC&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;EDWB: Mar 24, 2015 5:30:30 PM Code generation started.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;EDWB: Code generation time was 24694 ms.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;EDWB: project was successfully generated.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49562iCB0A191C3FDB592C/image-size/large?v=v2&amp;amp;px=999" title="Screen Shot 03-24-15 at 05.36 PM.PNG" alt="Screen Shot 03-24-15 at 05.36 PM.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2015 21:39:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Error-when-adding-ADC-component-KDS-Processor-Expert/m-p/318677#M14146</guid>
      <dc:creator>barbercolman</dc:creator>
      <dc:date>2015-03-24T21:39:29Z</dc:date>
    </item>
  </channel>
</rss>