<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Overheated problem of K60</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318356#M14090</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Would be possible that you send me your schematics?&lt;/P&gt;&lt;P&gt;Please check if you do not have any electrical short or wrong component?&lt;/P&gt;&lt;P&gt;What happens if you load a empty project, the board gets hot?&lt;/P&gt;&lt;P&gt;I believe that you are using a LQFP package, can you please check that there is not any solder short between the pins&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Jul 2014 21:17:56 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2014-07-29T21:17:56Z</dc:date>
    <item>
      <title>Overheated problem of K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318353#M14087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am using MK60FX512VLQ12 in bare-metal mode. Every 0.833ms it will perform ADC . The loop in the main() do some Key Scanning and&lt;/P&gt;&lt;P&gt;Uart Sending. No other features in its code. Now the K60 chip will be overheated(may be 60℃) after 20 minutes' running. If debug K60 with&lt;/P&gt;&lt;P&gt;J-link, it will be overheated(may be 90℃) in less time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The chip runs well and can be debugged.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; What could be the problem and how can I identify it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bests&lt;/P&gt;&lt;P&gt;Fukai from BeiJing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2014 09:11:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318353#M14087</guid>
      <dc:creator>wangfukai</dc:creator>
      <dc:date>2014-07-10T09:11:52Z</dc:date>
    </item>
    <item>
      <title>Re: Overheated problem of K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318354#M14088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fukai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the ambient temperature near the part?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you measure the current draw of the part when this happens?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you also post a schematic?&amp;nbsp; At least a snippet of the device and the power capacitors and other power supply circuitry?&amp;nbsp; That may help to provide some clues.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Chris &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2014 14:52:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318354#M14088</guid>
      <dc:creator>chris_brown</dc:creator>
      <dc:date>2014-07-10T14:52:16Z</dc:date>
    </item>
    <item>
      <title>Re: Overheated problem of K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318355#M14089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chris,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your kind help firstly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44980i707219A4493B44BC/image-size/large?v=v2&amp;amp;px=999" title="IMG_20140712_080528.jpg" alt="IMG_20140712_080528.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;That's how the cpu board should be used, in a box with other boards. Initially, I guess the over heated problem &lt;/P&gt;&lt;P&gt;was caused by the&amp;nbsp; power board. There is a big AC/DC module on power board.&lt;/P&gt;&lt;P&gt;So I pluged the CPU board out and soldered a 5V power on LM1117 pin directly as showed after.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44981i2CD4121D4802033E/image-size/large?v=v2&amp;amp;px=999" title="IMG_20140712_080541.jpg" alt="IMG_20140712_080541.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And the over heated problem still exist. The &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;ambient temperature&lt;/SPAN&gt; is 27℃ and we have an air-conditioner in our school lab&lt;/P&gt;&lt;P&gt;so this should not be the cause.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I measured current of the whole CPU&amp;nbsp; board and it is 0.341A.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are four modules on the CPU board:&amp;nbsp; Internet port, RS485 port, EEPROM, IO port. But none of these modules were&lt;/P&gt;&lt;P&gt;used in the project code. The CPU only do A/D conversation every 0.833ms with the internal ADC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Fukai&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Jul 2014 01:06:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318355#M14089</guid>
      <dc:creator>wangfukai</dc:creator>
      <dc:date>2014-07-12T01:06:38Z</dc:date>
    </item>
    <item>
      <title>Re: Overheated problem of K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318356#M14090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Would be possible that you send me your schematics?&lt;/P&gt;&lt;P&gt;Please check if you do not have any electrical short or wrong component?&lt;/P&gt;&lt;P&gt;What happens if you load a empty project, the board gets hot?&lt;/P&gt;&lt;P&gt;I believe that you are using a LQFP package, can you please check that there is not any solder short between the pins&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jul 2014 21:17:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318356#M14090</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2014-07-29T21:17:56Z</dc:date>
    </item>
    <item>
      <title>Re: Overheated problem of K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318357#M14091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vicente,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I soldered another board and no overheat problem occurred. So that MCU on the overheat&amp;nbsp; board&lt;/P&gt;&lt;P&gt;may has something wrong.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I checked the MCU and no pins was shorted. And the MCU still can be linked with Jlink.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; So, it is strange. The temperature in the box which contains the MCU board is a little bit hot, So I guess&lt;/P&gt;&lt;P&gt;may that cause the MCU to be destroyed but not totally destroyed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;Fukai&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2014 02:20:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318357#M14091</guid>
      <dc:creator>wangfukai</dc:creator>
      <dc:date>2014-07-30T02:20:25Z</dc:date>
    </item>
    <item>
      <title>Re: Overheated problem of K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318358#M14092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, you can check the impedance between the good part and the failed part, I do not know if this is possible but what happened if you place a new MCU on the failed board, I am thinking that the problem is on the board (hardware), probably a wrong or missing component. If you place a new MCU and the board still did not work, I will check the hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Aug 2014 18:49:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318358#M14092</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2014-08-01T18:49:59Z</dc:date>
    </item>
    <item>
      <title>Re: Overheated problem of K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318359#M14093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vicente,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, the board was good in the beginning. And days later it went to wrong so I soldered another MCU on the board. It keeped well&lt;/P&gt;&lt;P&gt;for another days and then went wrong again. &lt;/P&gt;&lt;P&gt;So I suppose the box's high temperature&amp;nbsp; is the cause.&lt;/P&gt;&lt;P&gt;I chang another new board with new MCU and check what will happen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Fukai&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Aug 2014 23:55:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318359#M14093</guid>
      <dc:creator>wangfukai</dc:creator>
      <dc:date>2014-08-01T23:55:41Z</dc:date>
    </item>
    <item>
      <title>Re: Overheated problem of K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318360#M14094</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fukai:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;300mA current is large enough to make chip overheated.&lt;/P&gt;&lt;P&gt;Maybe something short, you could check every pin to clear the short pin to GND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you use internal USB regulator module? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dawei You（尤大为）&lt;/P&gt;&lt;P&gt;Mobile: +86 13675169919&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Aug 2014 14:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318360#M14094</guid>
      <dc:creator>daweiyou</dc:creator>
      <dc:date>2014-08-03T14:33:31Z</dc:date>
    </item>
    <item>
      <title>Re: Overheated problem of K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318361#M14095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dawei,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I thought I find the problem. The box we use is made of metal and it let two boards be shorted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Fukai&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Aug 2014 00:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Overheated-problem-of-K60/m-p/318361#M14095</guid>
      <dc:creator>wangfukai</dc:creator>
      <dc:date>2014-08-04T00:28:13Z</dc:date>
    </item>
  </channel>
</rss>