<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 problem using two serial devices at the same time</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-using-two-serial-devices-at-the-same-time/m-p/317724#M14072</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the TWR-K60F120M with the TWR-SER board using both available serial ports at the same time.&amp;nbsp; I have the shell running on the OSJTAG port without problem (ttyf) now I'm trying to use the serial port (ttyd) for a custom protocol, but for now, I'm just opening and writing a test string to the port.&amp;nbsp;&amp;nbsp; The open and write are not returning any errors, but the test strings are not what I'm reading from the TWR-SER connector.&amp;nbsp; Instead, I'm seeing a duplicate of all the shell output from ttyf.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any thoughts would be appreciated.&amp;nbsp; I don't understand why I'm seeing this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Jul 2014 12:39:19 GMT</pubDate>
    <dc:creator>tschtj</dc:creator>
    <dc:date>2014-07-09T12:39:19Z</dc:date>
    <item>
      <title>problem using two serial devices at the same time</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-using-two-serial-devices-at-the-same-time/m-p/317724#M14072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the TWR-K60F120M with the TWR-SER board using both available serial ports at the same time.&amp;nbsp; I have the shell running on the OSJTAG port without problem (ttyf) now I'm trying to use the serial port (ttyd) for a custom protocol, but for now, I'm just opening and writing a test string to the port.&amp;nbsp;&amp;nbsp; The open and write are not returning any errors, but the test strings are not what I'm reading from the TWR-SER connector.&amp;nbsp; Instead, I'm seeing a duplicate of all the shell output from ttyf.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any thoughts would be appreciated.&amp;nbsp; I don't understand why I'm seeing this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2014 12:39:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-using-two-serial-devices-at-the-same-time/m-p/317724#M14072</guid>
      <dc:creator>tschtj</dc:creator>
      <dc:date>2014-07-09T12:39:19Z</dc:date>
    </item>
    <item>
      <title>Re: problem using two serial devices at the same time</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-using-two-serial-devices-at-the-same-time/m-p/317725#M14073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;Not all tower designs (form, fit, functionality) are identical.&amp;nbsp; Some Towers have independent UARTS going to the OSJTAG(debugger interface) and TWR-SER card.&amp;nbsp; Other Towers have one UART going to both.&lt;/P&gt;&lt;P&gt;The TWR-K60F120M is one of the latter cases where the UART5/ttyf is going to both the OSJTAG and TWR-SER card.&amp;nbsp; This has advantage of not having to change MQX code to use one or the other serial interface but has a negative that you only have access to one UART.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2014 15:02:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/problem-using-two-serial-devices-at-the-same-time/m-p/317725#M14073</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2014-07-09T15:02:45Z</dc:date>
    </item>
  </channel>
</rss>