<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Problem with pin reset on MCU MKL25Z128VLK4.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-pin-reset-on-MCU-MKL25Z128VLK4/m-p/317393#M14048</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I started a new project with a similar design to Freedom KL25Z OPENSDA, my board not working Correctly, the MKL25Z128VLK4 is always reset, the pin 42 is pulled with 10 K to VCC, &lt;/P&gt;&lt;P&gt;the extern oscillator 8 MHz not clock, the waveform on pin reset (42) is similar to ramp at frequency 32KHz. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jun 2014 13:07:18 GMT</pubDate>
    <dc:creator>sacchettigiampa</dc:creator>
    <dc:date>2014-06-11T13:07:18Z</dc:date>
    <item>
      <title>Problem with pin reset on MCU MKL25Z128VLK4.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-pin-reset-on-MCU-MKL25Z128VLK4/m-p/317393#M14048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I started a new project with a similar design to Freedom KL25Z OPENSDA, my board not working Correctly, the MKL25Z128VLK4 is always reset, the pin 42 is pulled with 10 K to VCC, &lt;/P&gt;&lt;P&gt;the extern oscillator 8 MHz not clock, the waveform on pin reset (42) is similar to ramp at frequency 32KHz. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 13:07:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-pin-reset-on-MCU-MKL25Z128VLK4/m-p/317393#M14048</guid>
      <dc:creator>sacchettigiampa</dc:creator>
      <dc:date>2014-06-11T13:07:18Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with pin reset on MCU MKL25Z128VLK4.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-pin-reset-on-MCU-MKL25Z128VLK4/m-p/317394#M14049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The signal on the reset pin is normal in new devices. Device is reset because of the watchdog or illegal instruction fault.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To eliminate this, the first thing to do with a new device is a mass erase. There are several options to do a mass erase, depending on the IDE + programming tool you use.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And about the external oscillator, it has to be enabled first by code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 15:11:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-pin-reset-on-MCU-MKL25Z128VLK4/m-p/317394#M14049</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-06-11T15:11:44Z</dc:date>
    </item>
  </channel>
</rss>