<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックUse of system mode controller (SMC) in Kinetis</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-system-mode-controller-SMC-in-Kinetis/m-p/317388#M14046</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;question 1: I have a K60: MK60DN512VLL10. I have a bareboard project with PE enabled. I have a for loop that checks for several modules in a round robin fashion. I was thinking if there is a possibility to use SMC if possible. I see chapter 14 of reference manual explains this. But is there anywhere that shows me how I can set this up in my ProcessorExpert?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;question 2: In chapter 15 of manual, it is talking about power management controller. I need to check if Kinetis is low voltage or high voltage. I see that 15.3 talks about low-voltage detect system, but is there any high-voltage detect system?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jun 2014 17:24:11 GMT</pubDate>
    <dc:creator>mehdikarimibiuk</dc:creator>
    <dc:date>2014-06-11T17:24:11Z</dc:date>
    <item>
      <title>Use of system mode controller (SMC) in Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-system-mode-controller-SMC-in-Kinetis/m-p/317388#M14046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;question 1: I have a K60: MK60DN512VLL10. I have a bareboard project with PE enabled. I have a for loop that checks for several modules in a round robin fashion. I was thinking if there is a possibility to use SMC if possible. I see chapter 14 of reference manual explains this. But is there anywhere that shows me how I can set this up in my ProcessorExpert?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;question 2: In chapter 15 of manual, it is talking about power management controller. I need to check if Kinetis is low voltage or high voltage. I see that 15.3 talks about low-voltage detect system, but is there any high-voltage detect system?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 17:24:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-system-mode-controller-SMC-in-Kinetis/m-p/317388#M14046</guid>
      <dc:creator>mehdikarimibiuk</dc:creator>
      <dc:date>2014-06-11T17:24:11Z</dc:date>
    </item>
    <item>
      <title>Re: Use of system mode controller (SMC) in Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-system-mode-controller-SMC-in-Kinetis/m-p/317389#M14047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do not think there is PMC(power management controller) bean in PE, if you want to control Kinetis to enter low mode for example VLPR, LLS or VLLSx mode, I suggest you refer to application note&amp;nbsp; an4470 and it's corresponding example code.&lt;/P&gt;&lt;P&gt;You can download an4470 and an4470sw from the website:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;A class="jive-link-external-small" href="http://tinyurl.com/l2p5b7b"&gt;http://tinyurl.com/l2p5b7b&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your second question, for Kinetis K family, the maximum power voltage is 3.6V, we assume that the Kinetis family is powered by battery in hand-hold application, when battery&amp;nbsp; runs out of energy, the voltage will drop, this is most cases. So we take a lot effort to design for lower power application. but we do not take a lot of effort for the High voltage application, so there is not high-voltage detect system.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 09:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-of-system-mode-controller-SMC-in-Kinetis/m-p/317389#M14047</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2014-06-12T09:04:34Z</dc:date>
    </item>
  </channel>
</rss>