<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: USB Enumeration Pass through</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Enumeration-Pass-through/m-p/316951#M13986</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank for your reply, from your response we installed code warrior studio and created a MQX 4.1 project but on the IDE &lt;/P&gt;&lt;P&gt;we are unable to select the support of USB host and device mode at a time. But in our project we need both support for &lt;/P&gt;&lt;P&gt;both USB in the host and device mode.So please give me some suggestions regarding this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Siva Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Jun 2014 05:04:25 GMT</pubDate>
    <dc:creator>s_v_s_kumar</dc:creator>
    <dc:date>2014-06-13T05:04:25Z</dc:date>
    <item>
      <title>USB Enumeration Pass through</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Enumeration-Pass-through/m-p/316949#M13984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on a project please guide us is our requirement is achievable or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would like to use k70 in our project. The K70 has USB interface can be acted as host and gadget.&lt;/P&gt;&lt;P&gt;Is the enumeration of the host can be passed to gadget driver dynamically?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For better understanding see the following example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K70 is connected to PC as a gadget and any USB device(3G/Wi-Fi dongle) is connected to the K70 then the&lt;/P&gt;&lt;P&gt;enumeration from the K70 host should be passed to gadget driver dynamically.&lt;/P&gt;&lt;P&gt;The PC should see the USB device(3G/Wi-Fi dongle) is it possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it can be done how complex in making it work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Siva Kumar &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 05:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Enumeration-Pass-through/m-p/316949#M13984</guid>
      <dc:creator>s_v_s_kumar</dc:creator>
      <dc:date>2014-06-11T05:48:20Z</dc:date>
    </item>
    <item>
      <title>Re: USB Enumeration Pass through</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Enumeration-Pass-through/m-p/316950#M13985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you very much for your focus on Freescale Kinetis product. I am glad to provide service for you.&lt;/P&gt;&lt;P&gt;After I've had a look through your questions, I think your idea of K70 act "HUB" role could work out.&lt;/P&gt;&lt;P&gt;We can find that K70 has two USB OTG controllers which are USBOTG and USBHS and these USB OTG controllers both could work in device mode or host mode.&lt;/P&gt;&lt;P&gt;So it's available to K70 act as device to PC, meanwhile K70 act as host to other peripheral USB devices.&lt;/P&gt;&lt;P&gt;However it need use the both of USB OTG controllers in K70 to achieve this implementation.&lt;/P&gt;&lt;P&gt;And You should integrate device_mode and host_mode demo code which are provided from FSL USB Stack, beause there's no similar demo in FSL USB Stack.&lt;/P&gt;&lt;P&gt;FSL USB stack information link as follow:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 06:04:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Enumeration-Pass-through/m-p/316950#M13985</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-06-12T06:04:22Z</dc:date>
    </item>
    <item>
      <title>Re: USB Enumeration Pass through</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Enumeration-Pass-through/m-p/316951#M13986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank for your reply, from your response we installed code warrior studio and created a MQX 4.1 project but on the IDE &lt;/P&gt;&lt;P&gt;we are unable to select the support of USB host and device mode at a time. But in our project we need both support for &lt;/P&gt;&lt;P&gt;both USB in the host and device mode.So please give me some suggestions regarding this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Siva Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jun 2014 05:04:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Enumeration-Pass-through/m-p/316951#M13986</guid>
      <dc:creator>s_v_s_kumar</dc:creator>
      <dc:date>2014-06-13T05:04:25Z</dc:date>
    </item>
    <item>
      <title>Re: USB Enumeration Pass through</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Enumeration-Pass-through/m-p/316952#M13987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Kinetis support team only handle the questions of bare board that without run with any system.&lt;/P&gt;&lt;P&gt;So I've already moved your question to MQX team and I'm sorry for bringing any inconvenience to you.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jun 2014 08:54:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Enumeration-Pass-through/m-p/316952#M13987</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-06-13T08:54:37Z</dc:date>
    </item>
  </channel>
</rss>