<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFRDM-K64F reading the ADC</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-reading-the-ADC/m-p/316575#M13933</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Im new to the K64F, I have some programming background mostly C, and C++, and I need a little help or at least some direction on where to start, code wise, so I can display or capture information directly from the on board ADC. As a side note I would like to read from the Magnetometer, and accelerometer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Jul 2014 13:41:52 GMT</pubDate>
    <dc:creator>tedbedard</dc:creator>
    <dc:date>2014-07-07T13:41:52Z</dc:date>
    <item>
      <title>FRDM-K64F reading the ADC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-reading-the-ADC/m-p/316575#M13933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Im new to the K64F, I have some programming background mostly C, and C++, and I need a little help or at least some direction on where to start, code wise, so I can display or capture information directly from the on board ADC. As a side note I would like to read from the Magnetometer, and accelerometer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jul 2014 13:41:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-reading-the-ADC/m-p/316575#M13933</guid>
      <dc:creator>tedbedard</dc:creator>
      <dc:date>2014-07-07T13:41:52Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F reading the ADC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-reading-the-ADC/m-p/316576#M13934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ted,&lt;/P&gt;&lt;P&gt;Thank you very much for your focus on Freescale Kinetis product. I'm glad to provide service for you.&lt;/P&gt;&lt;P&gt;I'd like suggest you could find some documents about FRDM-K64F through the linke as follow and these documents could give you a quick overview of FRDM-K64F.&lt;/P&gt;&lt;P&gt;Next you should review the chapter about ADC module in reference manual and download the TWR-K64F120M' demo code.&lt;/P&gt;&lt;P&gt;At last, you could refer to ADC code in TWR-K64F120M' demo code and migrate to FRDM-K64, as the two board both use K64, so it's the migration work is easily.&lt;/P&gt;&lt;P&gt;Hope this reply help.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Aug 2014 06:40:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-reading-the-ADC/m-p/316576#M13934</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-08-01T06:40:19Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F reading the ADC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-reading-the-ADC/m-p/316577#M13935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ted&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See &lt;A _jive_internal="true" href="https://community.nxp.com/thread/322132" title="https://community.freescale.com/thread/322132"&gt;https://community.freescale.com/thread/322132&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It includes ADC sampling using interrupts as well as DMA (with options to perform a DMA controlled digital delay line between an ADC input and DAC output, plus to save the ADC samples to a WAV file on the SD card).&lt;/P&gt;&lt;P&gt;The accelerometer is also supported in either free-running mode (back-to-back I2C reading) or in interrupt driven mode - options are available to use the accelerometer input to control PWM outputs to adjust RGB colour or to use it as the input to USB tilt-mouse.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Supports FRDM-K64F to build with CW10.x, KDS, IAR, Keil, Rowley, Coo Cox, Atollic or standalone GCC, and simulates the K64 and FRDM-K64F using VisualStudio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Aug 2014 12:39:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-reading-the-ADC/m-p/316577#M13935</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-08-01T12:39:19Z</dc:date>
    </item>
  </channel>
</rss>