<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K22 Flexbus CSPMCR Registers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus-CSPMCR-Registers/m-p/316342#M13931</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the Flexbus of a K22 hooked up to an OLED display through FB_AD[7:0].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not convinced that I've configured the Flexbus peripheral correctly as I'm seeing spurious pulses on the FB_AD[0] signal when looking at the bus on a logic analyser.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My code so far is...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Configure the FlexBus chip select&lt;/P&gt;&lt;P&gt;FB-&amp;gt;CS[0].CSAR = EBI_BASE_ADDRESS;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // 0x60000000&lt;/P&gt;&lt;P&gt;// Set up the port size to 8bit&lt;/P&gt;&lt;P&gt;FB-&amp;gt;CS[0].CSCR = FB_CSCR_PS(1) | FB_CSCR_AA_MASK | FB_CSCR_WS(1) | FB_CSCR_BLS_MASK;&lt;/P&gt;&lt;P&gt;// Set up the chip select mask register&lt;/P&gt;&lt;P&gt;FB-&amp;gt;CS[0].CSMR = FB_CSMR_V_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I need to set FB_BE_7_0 = 1 and TSIZ[1:0] = 0b01 in the FB_CSPMCR register in order for correct 8-bit operation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Kev&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Jun 2014 21:11:30 GMT</pubDate>
    <dc:creator>weblar</dc:creator>
    <dc:date>2014-06-09T21:11:30Z</dc:date>
    <item>
      <title>K22 Flexbus CSPMCR Registers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus-CSPMCR-Registers/m-p/316342#M13931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the Flexbus of a K22 hooked up to an OLED display through FB_AD[7:0].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not convinced that I've configured the Flexbus peripheral correctly as I'm seeing spurious pulses on the FB_AD[0] signal when looking at the bus on a logic analyser.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My code so far is...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Configure the FlexBus chip select&lt;/P&gt;&lt;P&gt;FB-&amp;gt;CS[0].CSAR = EBI_BASE_ADDRESS;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // 0x60000000&lt;/P&gt;&lt;P&gt;// Set up the port size to 8bit&lt;/P&gt;&lt;P&gt;FB-&amp;gt;CS[0].CSCR = FB_CSCR_PS(1) | FB_CSCR_AA_MASK | FB_CSCR_WS(1) | FB_CSCR_BLS_MASK;&lt;/P&gt;&lt;P&gt;// Set up the chip select mask register&lt;/P&gt;&lt;P&gt;FB-&amp;gt;CS[0].CSMR = FB_CSMR_V_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I need to set FB_BE_7_0 = 1 and TSIZ[1:0] = 0b01 in the FB_CSPMCR register in order for correct 8-bit operation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Kev&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 21:11:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus-CSPMCR-Registers/m-p/316342#M13931</guid>
      <dc:creator>weblar</dc:creator>
      <dc:date>2014-06-09T21:11:30Z</dc:date>
    </item>
    <item>
      <title>Re: K22 Flexbus CSPMCR Registers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus-CSPMCR-Registers/m-p/316343#M13932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Never mind, managed to fix the issue by setting the port size to 32bit but only using the lower 8 bits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The display now works correctly with no extra tinkering.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 08:21:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus-CSPMCR-Registers/m-p/316343#M13932</guid>
      <dc:creator>weblar</dc:creator>
      <dc:date>2014-06-10T08:21:43Z</dc:date>
    </item>
  </channel>
</rss>