<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: USB0_DP and USB0_DM when USB not used - K60</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB0-DP-and-USB0-DM-when-USB-not-used-K60/m-p/315871#M13857</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;just put both of them to GND is OK.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Jul 2014 05:14:14 GMT</pubDate>
    <dc:creator>wenlongzhang</dc:creator>
    <dc:date>2014-07-04T05:14:14Z</dc:date>
    <item>
      <title>USB0_DP and USB0_DM when USB not used - K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB0-DP-and-USB0-DM-when-USB-not-used-K60/m-p/315870#M13856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On a K60F what should we do with the USB0_DP and USB0_DM pins when we aren't using the USB peripheral?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There doesn't seem to be any guidance in the datasheet or user manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was thinking that we would pull them down to GND lightly.&amp;nbsp; Or should we pull them up lightly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jul 2014 05:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB0-DP-and-USB0-DM-when-USB-not-used-K60/m-p/315870#M13856</guid>
      <dc:creator>igw</dc:creator>
      <dc:date>2014-07-04T05:02:15Z</dc:date>
    </item>
    <item>
      <title>Re: USB0_DP and USB0_DM when USB not used - K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB0-DP-and-USB0-DM-when-USB-not-used-K60/m-p/315871#M13857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;just put both of them to GND is OK.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jul 2014 05:14:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB0-DP-and-USB0-DM-when-USB-not-used-K60/m-p/315871#M13857</guid>
      <dc:creator>wenlongzhang</dc:creator>
      <dc:date>2014-07-04T05:14:14Z</dc:date>
    </item>
    <item>
      <title>Re: USB0_DP and USB0_DM when USB not used - K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB0-DP-and-USB0-DM-when-USB-not-used-K60/m-p/315872#M13858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ian,&lt;/P&gt;&lt;P&gt;Thank you very much for your focus on Freescale Kinetis product. I'm glad to provide service for you.&lt;/P&gt;&lt;P&gt;It's ok to pull the USB0_DP and USB0_DM pins down to GND.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jul 2014 02:58:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB0-DP-and-USB0-DM-when-USB-not-used-K60/m-p/315872#M13858</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-07-08T02:58:44Z</dc:date>
    </item>
  </channel>
</rss>