<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK60 UART interrupt is stuck</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-UART-interrupt-is-stuck/m-p/315592#M13825</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;My UART interface RX stream is stuck and no new RX interrupt&amp;nbsp; is received for any attempt to drive input.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;I &lt;/SPAN&gt;experience&lt;SPAN style="font-size: 10pt;"&gt; a UART overflow, caused by interrupt long latency, which leaves the system with no active interrupt but with a char in the buffer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;This prevents from new char to be received. the only thing that "releases" the UART interface is D read.&lt;/P&gt;&lt;P&gt;Following this read the interface is released and the RX flow runs once again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The UART statuses doesn't apply to any reasonable cause.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See UART status log below:&lt;/P&gt;&lt;P&gt;4006A000: 00 36 00 2C C8 40 00 XX 00 00 08 00 00 00 00 AA &lt;/P&gt;&lt;P&gt;4006A010: 22 00 C5 00 00 01 00 AA 00 00 00 0A 00 01 00 00 &lt;/P&gt;&lt;P&gt;4006A020: AA 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 &lt;/P&gt;&lt;P&gt;4006A030: 00 00 AA AA AA AA AA AA AA AA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that the XX located in 4006A007 is the D register. Once this address is called the block is released.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tnx, &lt;/P&gt;&lt;P&gt;Gerry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Jul 2014 10:12:52 GMT</pubDate>
    <dc:creator>gerry26</dc:creator>
    <dc:date>2014-07-03T10:12:52Z</dc:date>
    <item>
      <title>K60 UART interrupt is stuck</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-UART-interrupt-is-stuck/m-p/315592#M13825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;My UART interface RX stream is stuck and no new RX interrupt&amp;nbsp; is received for any attempt to drive input.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;I &lt;/SPAN&gt;experience&lt;SPAN style="font-size: 10pt;"&gt; a UART overflow, caused by interrupt long latency, which leaves the system with no active interrupt but with a char in the buffer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;This prevents from new char to be received. the only thing that "releases" the UART interface is D read.&lt;/P&gt;&lt;P&gt;Following this read the interface is released and the RX flow runs once again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The UART statuses doesn't apply to any reasonable cause.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See UART status log below:&lt;/P&gt;&lt;P&gt;4006A000: 00 36 00 2C C8 40 00 XX 00 00 08 00 00 00 00 AA &lt;/P&gt;&lt;P&gt;4006A010: 22 00 C5 00 00 01 00 AA 00 00 00 0A 00 01 00 00 &lt;/P&gt;&lt;P&gt;4006A020: AA 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 &lt;/P&gt;&lt;P&gt;4006A030: 00 00 AA AA AA AA AA AA AA AA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that the XX located in 4006A007 is the D register. Once this address is called the block is released.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tnx, &lt;/P&gt;&lt;P&gt;Gerry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jul 2014 10:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-UART-interrupt-is-stuck/m-p/315592#M13825</guid>
      <dc:creator>gerry26</dc:creator>
      <dc:date>2014-07-03T10:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: K60 UART interrupt is stuck</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-UART-interrupt-is-stuck/m-p/315593#M13826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Gerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When an overrun takes place the overrun flag must be correctly cleared otherwise the UART receiver will not process further reception.&lt;/P&gt;&lt;P&gt;Please see the following with explanation of how to reset it (towards the end of the thread): &lt;A href="https://community.nxp.com/thread/326104"&gt;Lost UART interrupt on MK60DN512xxx10&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jul 2014 16:15:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-UART-interrupt-is-stuck/m-p/315593#M13826</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-07-04T16:15:19Z</dc:date>
    </item>
  </channel>
</rss>