<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: UARTx_C2 send break?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UARTx-C2-send-break/m-p/315097#M13775</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you set the SBK bit the UART will continuously send break characeters until you remove the bit. Then it will complete sending the break character that it was in the process of sending before returning to the idle line state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 07 Jun 2014 19:06:07 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-06-07T19:06:07Z</dc:date>
    <item>
      <title>UARTx_C2 send break?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UARTx-C2-send-break/m-p/315096#M13774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For K60, the UARTx_C2 SBK bit is used to send break.&lt;/P&gt;&lt;P&gt;Does it mean when I set the SBK bit, it will send break continuously until I clear the SBK bit?&lt;/P&gt;&lt;P&gt;Or it means after SBK is set, it only send 10, 11, 12, 13 or 14 logic 0s no matter if SBK is cleared or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 21:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UARTx-C2-send-break/m-p/315096#M13774</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2014-06-05T21:07:45Z</dc:date>
    </item>
    <item>
      <title>Re: UARTx_C2 send break?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UARTx-C2-send-break/m-p/315097#M13775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you set the SBK bit the UART will continuously send break characeters until you remove the bit. Then it will complete sending the break character that it was in the process of sending before returning to the idle line state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Jun 2014 19:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UARTx-C2-send-break/m-p/315097#M13775</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-06-07T19:06:07Z</dc:date>
    </item>
    <item>
      <title>Re: UARTx_C2 send break?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UARTx-C2-send-break/m-p/315098#M13776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel chai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Thank you for your question in our communty.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; As our reference manual said,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="59.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44454i7D1E838B6642928E/image-size/large?v=v2&amp;amp;px=999" role="button" title="59.jpg" alt="59.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="60.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44404iE5E8BD1A95BFF27E/image-size/large?v=v2&amp;amp;px=999" role="button" title="60.jpg" alt="60.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;so, it will continuoulsly send break until you clear the SBK bit.&lt;/P&gt;&lt;P&gt;Wish my answer helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact with me!&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 09:14:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UARTx-C2-send-break/m-p/315098#M13776</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2014-06-10T09:14:11Z</dc:date>
    </item>
  </channel>
</rss>