<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Does anyone know if configuring the FRDM-K64F FTM ( flexible timer module) to use an external clock that if the external clock period can be infinite.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-anyone-know-if-configuring-the-FRDM-K64F-FTM-flexible-timer/m-p/315036#M13769</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In theory it is infinite, for your specific case I don't think you will face any problem using your clock source (4,000/60=66.66Hz).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Jun 2014 21:17:47 GMT</pubDate>
    <dc:creator>apanecatl</dc:creator>
    <dc:date>2014-06-05T21:17:47Z</dc:date>
    <item>
      <title>Does anyone know if configuring the FRDM-K64F FTM ( flexible timer module) to use an external clock that if the external clock period can be infinite.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-anyone-know-if-configuring-the-FRDM-K64F-FTM-flexible-timer/m-p/315035#M13768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need clock the FTM with an external clock that is driven off of a magnetic pickup mounted to a shaft of a motor.&amp;nbsp; This motor rotates from&amp;nbsp; equal to 0 rpm to 4000 rpm.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 15:51:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-anyone-know-if-configuring-the-FRDM-K64F-FTM-flexible-timer/m-p/315035#M13768</guid>
      <dc:creator>darringarrett</dc:creator>
      <dc:date>2014-06-05T15:51:10Z</dc:date>
    </item>
    <item>
      <title>Re: Does anyone know if configuring the FRDM-K64F FTM ( flexible timer module) to use an external clock that if the external clock period can be infinite.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-anyone-know-if-configuring-the-FRDM-K64F-FTM-flexible-timer/m-p/315036#M13769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In theory it is infinite, for your specific case I don't think you will face any problem using your clock source (4,000/60=66.66Hz).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 21:17:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-anyone-know-if-configuring-the-FRDM-K64F-FTM-flexible-timer/m-p/315036#M13769</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2014-06-05T21:17:47Z</dc:date>
    </item>
    <item>
      <title>Re: Does anyone know if configuring the FRDM-K64F FTM ( flexible timer module) to use an external clock that if the external clock period can be infinite.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-anyone-know-if-configuring-the-FRDM-K64F-FTM-flexible-timer/m-p/315037#M13770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Pedro,&amp;nbsp; I am mostly concerned about the ability of the clock to function from 0 rpm and up from there.&amp;nbsp; So if the FTM can be clocked at very low frequencies then I could use this board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jun 2014 15:21:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-anyone-know-if-configuring-the-FRDM-K64F-FTM-flexible-timer/m-p/315037#M13770</guid>
      <dc:creator>darringarrett</dc:creator>
      <dc:date>2014-06-06T15:21:49Z</dc:date>
    </item>
  </channel>
</rss>