<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: I2C_LDD clock problem</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-LDD-clock-problem/m-p/315007#M13767</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid that the dividers of these two configuration do not allow to have a common frequency for the I2C module to work with. You can work with the FEE mode and use a external crystal or external reference clock which allows you to use the dividers to set a common frequency for the I2C module to work with both configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. It would be nice!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Jul 2014 21:06:52 GMT</pubDate>
    <dc:creator>adriancano</dc:creator>
    <dc:date>2014-07-07T21:06:52Z</dc:date>
    <item>
      <title>I2C_LDD clock problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-LDD-clock-problem/m-p/315006#M13766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using KL05 micro and I've a problem with setting of "Internal frequency" on I2C_LDD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've 2 clock path:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -CLOCK_CONFIG0: MCGIRCLK =20Mhz, bus 10Mhz FEI&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -CLOCK_CONFIG1: MCGIRCLK =2Mhz, bus 667khz BLPI&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On my code I need to use I2C in both configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to set init. value on "Timing dialog window" I can't choose a valid value because one value could be right for one clock and wrong for the other.&lt;/P&gt;&lt;P&gt;This is the message&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;EM&gt;&amp;nbsp;&amp;nbsp; "Timing setting failed in Clock configuration 0 - it is impossible to set the following items: initialization value"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;or&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;EM&gt; "Timing setting failed in Clock configuration 1 - it is impossible to set the following items: initialization value"&lt;/EM&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, is it possible to use I2C with both config?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jul 2014 08:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-LDD-clock-problem/m-p/315006#M13766</guid>
      <dc:creator>gianlucap_</dc:creator>
      <dc:date>2014-07-02T08:15:15Z</dc:date>
    </item>
    <item>
      <title>Re: I2C_LDD clock problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-LDD-clock-problem/m-p/315007#M13767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid that the dividers of these two configuration do not allow to have a common frequency for the I2C module to work with. You can work with the FEE mode and use a external crystal or external reference clock which allows you to use the dividers to set a common frequency for the I2C module to work with both configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. It would be nice!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jul 2014 21:06:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-LDD-clock-problem/m-p/315007#M13767</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2014-07-07T21:06:52Z</dc:date>
    </item>
  </channel>
</rss>