<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Synchronize two FTMs in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Synchronize-two-FTMs/m-p/173919#M1374</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to figure out how I can do a software synchronization of FTM0 and FTM1 timers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It looks like I can write to FTMx_SYNC[SWSYNC] for each module and have them setup to reset the CNT value. &amp;nbsp;However, since that is two separate writes for FTM0 and FTM1 they likely wouldn't be exactly in sync.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It looks like I could probably use an external HW sync to drive both modules, but it would be easier if I could do it with a SW sync.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Oct 2011 21:53:22 GMT</pubDate>
    <dc:creator>MikeAdv</dc:creator>
    <dc:date>2011-10-12T21:53:22Z</dc:date>
    <item>
      <title>Synchronize two FTMs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Synchronize-two-FTMs/m-p/173919#M1374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to figure out how I can do a software synchronization of FTM0 and FTM1 timers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It looks like I can write to FTMx_SYNC[SWSYNC] for each module and have them setup to reset the CNT value. &amp;nbsp;However, since that is two separate writes for FTM0 and FTM1 they likely wouldn't be exactly in sync.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It looks like I could probably use an external HW sync to drive both modules, but it would be easier if I could do it with a SW sync.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2011 21:53:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Synchronize-two-FTMs/m-p/173919#M1374</guid>
      <dc:creator>MikeAdv</dc:creator>
      <dc:date>2011-10-12T21:53:22Z</dc:date>
    </item>
    <item>
      <title>Re: Synchronize two FTMs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Synchronize-two-FTMs/m-p/173920#M1375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;.... finally found what is probably the answer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Global Time Base (GTB) feature.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2011 22:10:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Synchronize-two-FTMs/m-p/173920#M1375</guid>
      <dc:creator>MikeAdv</dc:creator>
      <dc:date>2011-10-12T22:10:48Z</dc:date>
    </item>
  </channel>
</rss>