<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Hi All..I am using TWRK70F120M Tower Board and IAR Compiler. I want to write WORD and INT values to Flash and read them , but unable to do so. I am able to write string values into flash.Please let me know how to write WORD and INT values</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hi-All-I-am-using-TWRK70F120M-Tower-Board-and-IAR-Compiler-I/m-p/314254#M13705</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K70 can write only phrases to Flash (that is, 8 byes on an 8 bye boundary).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to write 8, 16 or 32 bit values you need to write them to a RAM buffer (phrase buffer) of the same size as the phrase to be programmed and always program a complete phrase. You can only program a phrase once and not reprogram a part of it so you can chose to either prepare multiple 8, 16 or 32 bit values in the phrase buffer until full and then write to Flash, or you can chose to write the value that you are interested in to occupy always a complete phrase buffer of its own.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Jun 2014 13:53:03 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-06-04T13:53:03Z</dc:date>
    <item>
      <title>Hi All..I am using TWRK70F120M Tower Board and IAR Compiler. I want to write WORD and INT values to Flash and read them , but unable to do so. I am able to write string values into flash.Please let me know how to write WORD and INT values</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hi-All-I-am-using-TWRK70F120M-Tower-Board-and-IAR-Compiler-I/m-p/314253#M13704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All..I am using TWRK70F120M Tower Board and IAR Compiler. I want to write WORD and INT values to Flash and read them , but unable to do so. I am able to write string values into flash.Please let me know how to write WORD and INT values&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jun 2014 12:31:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hi-All-I-am-using-TWRK70F120M-Tower-Board-and-IAR-Compiler-I/m-p/314253#M13704</guid>
      <dc:creator>snehahegde</dc:creator>
      <dc:date>2014-06-04T12:31:31Z</dc:date>
    </item>
    <item>
      <title>Re: Hi All..I am using TWRK70F120M Tower Board and IAR Compiler. I want to write WORD and INT values to Flash and read them , but unable to do so. I am able to write string values into flash.Please let me know how to write WORD and INT values</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hi-All-I-am-using-TWRK70F120M-Tower-Board-and-IAR-Compiler-I/m-p/314254#M13705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K70 can write only phrases to Flash (that is, 8 byes on an 8 bye boundary).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to write 8, 16 or 32 bit values you need to write them to a RAM buffer (phrase buffer) of the same size as the phrase to be programmed and always program a complete phrase. You can only program a phrase once and not reprogram a part of it so you can chose to either prepare multiple 8, 16 or 32 bit values in the phrase buffer until full and then write to Flash, or you can chose to write the value that you are interested in to occupy always a complete phrase buffer of its own.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jun 2014 13:53:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hi-All-I-am-using-TWRK70F120M-Tower-Board-and-IAR-Compiler-I/m-p/314254#M13705</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-06-04T13:53:03Z</dc:date>
    </item>
  </channel>
</rss>