<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: kinetis KL2x programming voltage @ 1.8V in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-KL2x-programming-voltage-1-8V/m-p/314088#M13694</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;got it done via CW10.x and P&amp;amp;E USB mulitlink but it cannot be done with OPENSDA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) KL26 freedom board, FRDM-KL26Z. REV B&lt;/P&gt;&lt;P&gt;remove the resistors of R2, R3, R4&lt;/P&gt;&lt;P&gt;cut the trace line below the jumpers of J13&lt;/P&gt;&lt;P&gt;pump in the power supply of 1.8V @ J5 pin, P3V3_KL26Z&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) KL25 freedom board, FRDM-KL25Z, REV E&lt;/P&gt;&lt;P&gt;Remove the resistor, R74, R81, R73&lt;/P&gt;&lt;P&gt;cut the trace line below the jumpers of J14,&lt;/P&gt;&lt;P&gt;pump in the power supply of 1.8V @ J4 pin, P3V3_KL25Z&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Heng&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Jun 2014 06:36:23 GMT</pubDate>
    <dc:creator>heng</dc:creator>
    <dc:date>2014-06-06T06:36:23Z</dc:date>
    <item>
      <title>kinetis KL2x programming voltage @ 1.8V</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-KL2x-programming-voltage-1-8V/m-p/314087#M13693</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to program the flash memory @1.8V VDD?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The tools that i have tried are&lt;/P&gt;&lt;P&gt;1) P&amp;amp;E (Green color) USB Multilink&lt;/P&gt;&lt;P&gt;2) P&amp;amp;E FX&amp;nbsp; (black color) USB mutlilinks&lt;/P&gt;&lt;P&gt;3) &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;J-link lite&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;All required at least around 2.7V VDD to download the binary into the flash memory of KL26 via SWD protocol.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried on IAR 7.20 and CW10.6 ID and have removed all the active components on the freedom board of KL26 (freedom REV B) but it still does not work.&lt;/P&gt;&lt;P&gt;The debugging and the flash programming only will only work when the VDD is around 2.7V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can we program the flash memory of kinetis KL2x @ 1.8V VDD?&lt;/P&gt;&lt;P&gt;From the RM, it show 1.71V to 3.6V with flash programable down to 1.71V with fully functional flash and analog peripherals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the tools we can use to program the flash memory @ 1.8V VDD?&lt;/P&gt;&lt;P&gt;Do we need to adjust a lower value of 10k and 4.7K of the pull-up resistors at reset pin and SWD_DIO pin respectively?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Heng&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jun 2014 03:57:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-KL2x-programming-voltage-1-8V/m-p/314087#M13693</guid>
      <dc:creator>heng</dc:creator>
      <dc:date>2014-06-04T03:57:36Z</dc:date>
    </item>
    <item>
      <title>Re: kinetis KL2x programming voltage @ 1.8V</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-KL2x-programming-voltage-1-8V/m-p/314088#M13694</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;got it done via CW10.x and P&amp;amp;E USB mulitlink but it cannot be done with OPENSDA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) KL26 freedom board, FRDM-KL26Z. REV B&lt;/P&gt;&lt;P&gt;remove the resistors of R2, R3, R4&lt;/P&gt;&lt;P&gt;cut the trace line below the jumpers of J13&lt;/P&gt;&lt;P&gt;pump in the power supply of 1.8V @ J5 pin, P3V3_KL26Z&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) KL25 freedom board, FRDM-KL25Z, REV E&lt;/P&gt;&lt;P&gt;Remove the resistor, R74, R81, R73&lt;/P&gt;&lt;P&gt;cut the trace line below the jumpers of J14,&lt;/P&gt;&lt;P&gt;pump in the power supply of 1.8V @ J4 pin, P3V3_KL25Z&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Heng&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jun 2014 06:36:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kinetis-KL2x-programming-voltage-1-8V/m-p/314088#M13694</guid>
      <dc:creator>heng</dc:creator>
      <dc:date>2014-06-06T06:36:23Z</dc:date>
    </item>
  </channel>
</rss>