<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: ADC offset</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313629#M13668</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Generally the Offset registers find usage in environment where the measured signals are not referenced with ground but with some other value. For example to measure a sinewave with amplitude +Vac to -Vac, the voltage would be scaled down on the hardware and provided an offset of Vdda/2 (MCU Analog Supply/2). The corresponding digital value would be written on the offset register. This in turn automatically gets adjusted in the result registers. As far as seeing 2090 instead of 2047 is concerned, it might be due to non linearity of resistor divider (tolerance levels) or a slight deviation of Vref (analog reference supply). The offset registers need to be written by the user, the value depending on the hardware configuration and application requirement.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Jul 2014 14:02:38 GMT</pubDate>
    <dc:creator>ankur_kala</dc:creator>
    <dc:date>2014-07-01T14:02:38Z</dc:date>
    <item>
      <title>ADC offset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313627#M13666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;I need to use the offset feature of the ADC. After the chip calibration I need the system calibration.&lt;/P&gt;&lt;P&gt;I read the result of conversion with my zero reference as a value: 2090, and it should be 2047 as midscale.&lt;/P&gt;&lt;P&gt;The offset register shows the value 0xFFFF. I don t find a good strategy for writing the right compensation value&lt;/P&gt;&lt;P&gt;there to produce what I want. I verify that writing 340 I have what I need but what is the logic?&lt;/P&gt;&lt;P&gt;I am using the 12 bits resolution&lt;/P&gt;&lt;P&gt;Thank You...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jun 2014 07:01:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313627#M13666</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2014-06-30T07:01:05Z</dc:date>
    </item>
    <item>
      <title>Re: ADC offset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313628#M13667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No one has answers??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Jul 2014 13:12:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313628#M13667</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2014-07-01T13:12:31Z</dc:date>
    </item>
    <item>
      <title>Re: ADC offset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313629#M13668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Generally the Offset registers find usage in environment where the measured signals are not referenced with ground but with some other value. For example to measure a sinewave with amplitude +Vac to -Vac, the voltage would be scaled down on the hardware and provided an offset of Vdda/2 (MCU Analog Supply/2). The corresponding digital value would be written on the offset register. This in turn automatically gets adjusted in the result registers. As far as seeing 2090 instead of 2047 is concerned, it might be due to non linearity of resistor divider (tolerance levels) or a slight deviation of Vref (analog reference supply). The offset registers need to be written by the user, the value depending on the hardware configuration and application requirement.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Jul 2014 14:02:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313629#M13668</guid>
      <dc:creator>ankur_kala</dc:creator>
      <dc:date>2014-07-01T14:02:38Z</dc:date>
    </item>
    <item>
      <title>Re: ADC offset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313630#M13669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Thank You for support. I see I can write to the offset register a value of 340 and I will read 2048, so the compensation is got. But rather than try some values I need to calculate the reasonable offset for getting a reading of 2047 when the input is my 0, that is &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 12px; background-color: #f6f6f6;"&gt;MCU Analog Supply/2&lt;/SPAN&gt;. So the question is if I read 2090 but I would like to read with the same input 2047 what is the value to write in the offset register? I am using now 12 bits..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Jul 2014 14:51:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313630#M13669</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2014-07-01T14:51:20Z</dc:date>
    </item>
    <item>
      <title>Re: ADC offset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313631#M13670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pietro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;The formatting of the offset register (ADCx_OFS) is different than the data result register (ADCx_Rn). The data held in the offset register value should be written left-justified in 2's complement form. The OFS[15] bit indicates the sign (positive or negative) of the offset value. In 12-bit single-ended mode, the offset register bits OFS[&lt;/SPAN&gt;&lt;STRONG style="font-size: 10pt;"&gt;14:3&lt;/STRONG&gt;&lt;SPAN style="font-size: 10pt;"&gt;] are subtracted from Rn[&lt;/SPAN&gt;&lt;STRONG style="font-size: 10pt;"&gt;11:0&lt;/STRONG&gt;&lt;SPAN style="font-size: 10pt;"&gt;] and bits OFS[2:0] are ignored. When subtracting the value stored in OFS from the ADC result register, the binary weight of bits OFS[14:3] will correspond to those of Rn[11:0]. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Bryan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Jul 2014 14:58:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313631#M13670</guid>
      <dc:creator>bryancole-b4682</dc:creator>
      <dc:date>2014-07-01T14:58:51Z</dc:date>
    </item>
    <item>
      <title>Re: ADC offset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313632#M13671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;Now it is clear..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jul 2014 06:29:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-offset/m-p/313632#M13671</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2014-07-02T06:29:46Z</dc:date>
    </item>
  </channel>
</rss>