<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: does freescale provide library for kinetis? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-freescale-provide-library-for-kinetis/m-p/173879#M1365</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That is just a personnet opinion, but i don't like much PE like tools. It is for sure more flexible, but very hard to set up all the registers. I like much more a very good structured lib with tons of examples. However, maybe if i giv more time to PE i can get used to it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Oct 2011 06:45:54 GMT</pubDate>
    <dc:creator>EthernetHelp</dc:creator>
    <dc:date>2011-10-21T06:45:54Z</dc:date>
    <item>
      <title>does freescale provide library for kinetis?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-freescale-provide-library-for-kinetis/m-p/173875#M1361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I notice TI provide stellarisWare library for their stelleris arm MCU. the library is well designed and is very easy to use.does freescale also plan to develop the library for kinetis?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2011 20:09:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-freescale-provide-library-for-kinetis/m-p/173875#M1361</guid>
      <dc:creator>bluehacker</dc:creator>
      <dc:date>2011-10-12T20:09:46Z</dc:date>
    </item>
    <item>
      <title>Re: does freescale provide library for kinetis?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-freescale-provide-library-for-kinetis/m-p/173876#M1362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is a frustration for me as well...&lt;/P&gt;&lt;P&gt;Since there was no answer from Fresscale, I would assume the answer is "no".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Oct 2011 00:48:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-freescale-provide-library-for-kinetis/m-p/173876#M1362</guid>
      <dc:creator>ianr</dc:creator>
      <dc:date>2011-10-21T00:48:19Z</dc:date>
    </item>
    <item>
      <title>Re: does freescale provide library for kinetis?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-freescale-provide-library-for-kinetis/m-p/173877#M1363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am interested in knowing what users are really looking for in terms of supporting software for the Kinetis.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- freescale provides a kit of sample code for most peripherals on the K40 and K60 for CW and IAR (in the kit's notes it is defined as being various "bare-metal" example projects [KINETIS512_SC])&lt;/P&gt;&lt;P&gt;- freescale also provides complimentary OS, TCP/IP and USB stacks (which would cost up to $100'000 if they needed to be purchased)&lt;/P&gt;&lt;P&gt;- also a touch-sensing software suite (TSSSW) [this is the only package which is grouped under 'library']&lt;/P&gt;&lt;P&gt;- plus a driver suite (Processor Expert - PE_DRIVER_SUITE)&lt;/P&gt;&lt;P&gt;- as well as example projects built into CW&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;StellarisWare software (from TI) is also a set of functions to control peripherals on their chips, together with example projects.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What makes StellarisWare so much better and what is freescale missing with their support?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Oct 2011 02:41:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-freescale-provide-library-for-kinetis/m-p/173877#M1363</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-10-21T02:41:05Z</dc:date>
    </item>
    <item>
      <title>Re: does freescale provide library for kinetis?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-freescale-provide-library-for-kinetis/m-p/173878#M1364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can understand the frustration.....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It took Freescale 3 months via support tickets to actually acknowledge that the clock code for CW10 was broken (didn't address errata 2448).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It took awhile before CW was even supported.&amp;nbsp;&amp;nbsp; I think the issue was more of being able to find information.&amp;nbsp;&amp;nbsp;&amp;nbsp; I think everything is there,&amp;nbsp; its just tougher to find.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is another example:&amp;nbsp;&amp;nbsp;&amp;nbsp; There are a couple USB examples in the Kinetis_SC.&amp;nbsp;&amp;nbsp;&amp;nbsp; But it took me searching the forums for awhile to realize they have a full USB stack (under the health care stuff) that is more comprehensive.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Oct 2011 06:33:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-freescale-provide-library-for-kinetis/m-p/173878#M1364</guid>
      <dc:creator>emh203</dc:creator>
      <dc:date>2011-10-21T06:33:51Z</dc:date>
    </item>
    <item>
      <title>Re: does freescale provide library for kinetis?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-freescale-provide-library-for-kinetis/m-p/173879#M1365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That is just a personnet opinion, but i don't like much PE like tools. It is for sure more flexible, but very hard to set up all the registers. I like much more a very good structured lib with tons of examples. However, maybe if i giv more time to PE i can get used to it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Oct 2011 06:45:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/does-freescale-provide-library-for-kinetis/m-p/173879#M1365</guid>
      <dc:creator>EthernetHelp</dc:creator>
      <dc:date>2011-10-21T06:45:54Z</dc:date>
    </item>
  </channel>
</rss>