<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFlash KwikStik using J-Link GDBServer</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-KwikStik-using-J-Link-GDBServer/m-p/313180#M13614</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;When creating a project using CodeWarrior 10.5, a RAM and FLASH configuration are created.&amp;nbsp; Using the FLASH configuration when debugging an application on the KwikStik automatically flashes the program onto the target.&amp;nbsp; After a power cycle the program runs.&amp;nbsp; I want to be able to do this with Eclipse and J-Link GDBServer.&amp;nbsp; With Eclipse and GDBServer, I can debug my application on the target , but the program does not run after a power cycle.&amp;nbsp; Using J-Link Commander and examining memory, it does appear that the program has been flashed.&amp;nbsp; The stack address (0x00) and start address (0x04) are correct.&amp;nbsp; Is the program not booting because the bootmode is not configured correctly?&amp;nbsp; There are some steps performed by CodeWarrior that my Eclipse and GDBServer are not doing.&amp;nbsp; Any suggestions would help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Apr 2014 21:50:44 GMT</pubDate>
    <dc:creator>briancook</dc:creator>
    <dc:date>2014-04-09T21:50:44Z</dc:date>
    <item>
      <title>Flash KwikStik using J-Link GDBServer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-KwikStik-using-J-Link-GDBServer/m-p/313180#M13614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;When creating a project using CodeWarrior 10.5, a RAM and FLASH configuration are created.&amp;nbsp; Using the FLASH configuration when debugging an application on the KwikStik automatically flashes the program onto the target.&amp;nbsp; After a power cycle the program runs.&amp;nbsp; I want to be able to do this with Eclipse and J-Link GDBServer.&amp;nbsp; With Eclipse and GDBServer, I can debug my application on the target , but the program does not run after a power cycle.&amp;nbsp; Using J-Link Commander and examining memory, it does appear that the program has been flashed.&amp;nbsp; The stack address (0x00) and start address (0x04) are correct.&amp;nbsp; Is the program not booting because the bootmode is not configured correctly?&amp;nbsp; There are some steps performed by CodeWarrior that my Eclipse and GDBServer are not doing.&amp;nbsp; Any suggestions would help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Apr 2014 21:50:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-KwikStik-using-J-Link-GDBServer/m-p/313180#M13614</guid>
      <dc:creator>briancook</dc:creator>
      <dc:date>2014-04-09T21:50:44Z</dc:date>
    </item>
    <item>
      <title>Re: Flash KwikStik using J-Link GDBServer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-KwikStik-using-J-Link-GDBServer/m-p/313181#M13615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My issue was watchdog related.&amp;nbsp; I needed to disable the watchdog module in fewer clock cycles when I migrated from the KL46 to the K40.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Apr 2015 20:30:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-KwikStik-using-J-Link-GDBServer/m-p/313181#M13615</guid>
      <dc:creator>briancook</dc:creator>
      <dc:date>2015-04-09T20:30:45Z</dc:date>
    </item>
  </channel>
</rss>