<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Burnt two MK60FN1M0VLQ12 when plug in USB port in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Burnt-two-MK60FN1M0VLQ12-when-plug-in-USB-port/m-p/149012#M136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I know this thread is old, however for future reference to anyone that comes across it, take look at Linear Tech's App Note #88:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Ceramic Input Capacitors Can Cause Overvoltage Transients" by&lt;BR /&gt;Goran Perica.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cds.linear.com/docs/en/application-note/an88f.pdf" title="http://cds.linear.com/docs/en/application-note/an88f.pdf"&gt;http://cds.linear.com/docs/en/application-note/an88f.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;"A recent trend in the design of portable devices has been &lt;/P&gt;&lt;P&gt;to use ceramic capacitors to filter DC/DC converter inputs.&lt;/P&gt;&lt;P&gt;Ceramic capacitors are often chosen because of their &lt;/P&gt;&lt;P&gt;small size, low equivalent series resistance (ESR) and &lt;/P&gt;&lt;P&gt;high RMS current capability. Also, recently, designers have &lt;/P&gt;&lt;P&gt;been looking to ceramic capacitors due to shortages of &lt;/P&gt;&lt;P&gt;tantalum capacitors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, using ceramic capacitors for input filtering &lt;/P&gt;&lt;P&gt;can cause problems. Applying a voltage step to a ceramic &lt;/P&gt;&lt;P&gt;capacitor causes a large current surge that stores energy &lt;/P&gt;&lt;P&gt;in the inductances of the power leads. A large voltage &lt;/P&gt;&lt;P&gt;spike is created when the stored energy is transferred &lt;/P&gt;&lt;P&gt;from these inductances into the ceramic capacitor. These &lt;/P&gt;&lt;P&gt;voltage spikes can easily be twice the amplitude of the &lt;/P&gt;&lt;P&gt;input voltage step. ... "&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Jun 2014 15:24:42 GMT</pubDate>
    <dc:creator>bobpaddock</dc:creator>
    <dc:date>2014-06-03T15:24:42Z</dc:date>
    <item>
      <title>Burnt two MK60FN1M0VLQ12 when plug in USB port</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Burnt-two-MK60FN1M0VLQ12-when-plug-in-USB-port/m-p/149008#M132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have connected the USB pins to the connector as detail in the image. But I burn the uC everytime I connect the USB port to a computer (host). I do not know what went wrong. As far as I am concern the uC needed the incoming Vbus 5V and regulate into the proper Vout to power the internal USB module of the uC. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the problem was resolve when I replace the F8 ferrite bead with a 30R resistor. But I don't think this will solve the problem. Currently, I am not using the VOUT33 so loading at the output is not an issue. Was it due to the value of C32? The datasheet recommends a much larger cap (2uF), but surely, a lower cap should not cause it to load.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help and enlighten me on this. Thank you.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/118933iDAD353291015741D/image-size/large?v=v2&amp;amp;px=999" title="2614_2614.png" alt="2614_2614.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2012 02:10:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Burnt-two-MK60FN1M0VLQ12-when-plug-in-USB-port/m-p/149008#M132</guid>
      <dc:creator>kakiayam</dc:creator>
      <dc:date>2012-10-24T02:10:29Z</dc:date>
    </item>
    <item>
      <title>Re: Burnt two MK60FN1M0VLQ12 when plug in USB port</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Burnt-two-MK60FN1M0VLQ12-when-plug-in-USB-port/m-p/149009#M133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the same problem with my prototype card with PK60N512VLL100.&amp;nbsp; when i plug the USB link, the uC is hot, and the power current from the USB connector is about 110 mA (i add 33 Ohm on this line). The VOUT33 is 0 V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The decoupling capacitor is 4,7 uF on VOUT33.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And the USB-Device demo don't work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you if somebody have idea.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2012 15:32:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Burnt-two-MK60FN1M0VLQ12-when-plug-in-USB-port/m-p/149009#M133</guid>
      <dc:creator>ec0359</dc:creator>
      <dc:date>2012-10-31T15:32:49Z</dc:date>
    </item>
    <item>
      <title>Re: Burnt two MK60FN1M0VLQ12 when plug in USB port</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Burnt-two-MK60FN1M0VLQ12-when-plug-in-USB-port/m-p/149010#M134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;The high level view of your hardware connections seems to be right if you have ensured that the pull-up resistors on D+ and D- are tied to 3.3V, and not 5V. However, you could refer to the USB connection of a Freescale Board (Freedom) which is also powered by the USB ports; on this board, the GND and VBUS signals from USB port areconnected to ferrites, but they have internal resistance of 330 ohm. You can review these details on Freedom´s schematic, available at the following link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL25Z_SCH.pdf"&gt;www.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL25Z_SCH.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;Hope this information will be useful for you. Have a nice day.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2013 19:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Burnt-two-MK60FN1M0VLQ12-when-plug-in-USB-port/m-p/149010#M134</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2013-02-19T19:02:02Z</dc:date>
    </item>
    <item>
      <title>Re: Burnt two MK60FN1M0VLQ12 when plug in USB port</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Burnt-two-MK60FN1M0VLQ12-when-plug-in-USB-port/m-p/149011#M135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that adding capacitors to power line and connect power line to pin 5 of U7 with reduce the effect of over-voltage transients occur on the USB power line when hot plugging, that may help to prevent the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Of course choosing a higher serial resistance value at high frequency of ferrite will make a better result comparing to low value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Mar 2013 09:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Burnt-two-MK60FN1M0VLQ12-when-plug-in-USB-port/m-p/149011#M135</guid>
      <dc:creator>Dekiru</dc:creator>
      <dc:date>2013-03-25T09:00:50Z</dc:date>
    </item>
    <item>
      <title>Re: Burnt two MK60FN1M0VLQ12 when plug in USB port</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Burnt-two-MK60FN1M0VLQ12-when-plug-in-USB-port/m-p/149012#M136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I know this thread is old, however for future reference to anyone that comes across it, take look at Linear Tech's App Note #88:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Ceramic Input Capacitors Can Cause Overvoltage Transients" by&lt;BR /&gt;Goran Perica.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cds.linear.com/docs/en/application-note/an88f.pdf" title="http://cds.linear.com/docs/en/application-note/an88f.pdf"&gt;http://cds.linear.com/docs/en/application-note/an88f.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;"A recent trend in the design of portable devices has been &lt;/P&gt;&lt;P&gt;to use ceramic capacitors to filter DC/DC converter inputs.&lt;/P&gt;&lt;P&gt;Ceramic capacitors are often chosen because of their &lt;/P&gt;&lt;P&gt;small size, low equivalent series resistance (ESR) and &lt;/P&gt;&lt;P&gt;high RMS current capability. Also, recently, designers have &lt;/P&gt;&lt;P&gt;been looking to ceramic capacitors due to shortages of &lt;/P&gt;&lt;P&gt;tantalum capacitors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, using ceramic capacitors for input filtering &lt;/P&gt;&lt;P&gt;can cause problems. Applying a voltage step to a ceramic &lt;/P&gt;&lt;P&gt;capacitor causes a large current surge that stores energy &lt;/P&gt;&lt;P&gt;in the inductances of the power leads. A large voltage &lt;/P&gt;&lt;P&gt;spike is created when the stored energy is transferred &lt;/P&gt;&lt;P&gt;from these inductances into the ceramic capacitor. These &lt;/P&gt;&lt;P&gt;voltage spikes can easily be twice the amplitude of the &lt;/P&gt;&lt;P&gt;input voltage step. ... "&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jun 2014 15:24:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Burnt-two-MK60FN1M0VLQ12-when-plug-in-USB-port/m-p/149012#M136</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2014-06-03T15:24:42Z</dc:date>
    </item>
  </channel>
</rss>