<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックVbat &amp; RTC problems</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Vbat-RTC-problems/m-p/173865#M1359</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did the first pre-production with K60 micro.&lt;/P&gt;&lt;P&gt;some boards are ok.&lt;/P&gt;&lt;P&gt;In some other I have this problem:&lt;/P&gt;&lt;P&gt;I set date/time at the first power up. All ok.&lt;/P&gt;&lt;P&gt;I power down board.&lt;/P&gt;&lt;P&gt;At the next power up date/time remains with values i set at the first power up (RTC module stopped).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some considerations:&lt;/P&gt;&lt;P&gt;- 32K oscillator is ok&lt;/P&gt;&lt;P&gt;- Battery voltage ok (3V)&lt;/P&gt;&lt;P&gt;- Board Vcc 3.3V&lt;/P&gt;&lt;P&gt;- Vbat pin voltage is ok&lt;/P&gt;&lt;P&gt;- tested board with 100nF and 10uF between Vbat pin and GND&lt;/P&gt;&lt;P&gt;- 2 BAT54 diodes to decouple 3V from battery and 3.3V from board regulator&lt;/P&gt;&lt;P&gt;- If I supply RTC module with external 3.3V supply instead of 3V battery it's all ok&lt;/P&gt;&lt;P&gt;-&amp;nbsp;K60P144M100SF2 doc gives 1.71V as min.&amp;nbsp;RTC battery supply voltage. Using battery I have 3V-(BAT54 drop)=2.8V&lt;/P&gt;&lt;P&gt;- On&amp;nbsp;&lt;SPAN&gt;K60P144M100SF2 I found the min. value of&amp;nbsp;VRFVBAT (VBAT voltage required to retain the VBAT register file) as TBD&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas on how to solve the problem?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Corrado&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Jun 2012 17:19:43 GMT</pubDate>
    <dc:creator>Curro</dc:creator>
    <dc:date>2012-06-21T17:19:43Z</dc:date>
    <item>
      <title>Vbat &amp; RTC problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Vbat-RTC-problems/m-p/173865#M1359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did the first pre-production with K60 micro.&lt;/P&gt;&lt;P&gt;some boards are ok.&lt;/P&gt;&lt;P&gt;In some other I have this problem:&lt;/P&gt;&lt;P&gt;I set date/time at the first power up. All ok.&lt;/P&gt;&lt;P&gt;I power down board.&lt;/P&gt;&lt;P&gt;At the next power up date/time remains with values i set at the first power up (RTC module stopped).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some considerations:&lt;/P&gt;&lt;P&gt;- 32K oscillator is ok&lt;/P&gt;&lt;P&gt;- Battery voltage ok (3V)&lt;/P&gt;&lt;P&gt;- Board Vcc 3.3V&lt;/P&gt;&lt;P&gt;- Vbat pin voltage is ok&lt;/P&gt;&lt;P&gt;- tested board with 100nF and 10uF between Vbat pin and GND&lt;/P&gt;&lt;P&gt;- 2 BAT54 diodes to decouple 3V from battery and 3.3V from board regulator&lt;/P&gt;&lt;P&gt;- If I supply RTC module with external 3.3V supply instead of 3V battery it's all ok&lt;/P&gt;&lt;P&gt;-&amp;nbsp;K60P144M100SF2 doc gives 1.71V as min.&amp;nbsp;RTC battery supply voltage. Using battery I have 3V-(BAT54 drop)=2.8V&lt;/P&gt;&lt;P&gt;- On&amp;nbsp;&lt;SPAN&gt;K60P144M100SF2 I found the min. value of&amp;nbsp;VRFVBAT (VBAT voltage required to retain the VBAT register file) as TBD&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas on how to solve the problem?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Corrado&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jun 2012 17:19:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Vbat-RTC-problems/m-p/173865#M1359</guid>
      <dc:creator>Curro</dc:creator>
      <dc:date>2012-06-21T17:19:43Z</dc:date>
    </item>
    <item>
      <title>Re: Vbat &amp; RTC problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Vbat-RTC-problems/m-p/173866#M1360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First off, if you have Rev 0 chips (0M33Z) I will assume you have implemented the 100ohm workaround for e2666 latchup.&amp;nbsp; Insertion of coin cells has an inherently fast Vbat ramp.&amp;nbsp; As for the oscillator, the impedance of this whole circuit is VERY HIGH, so I might suspect layout leakage/noise/capacitance, AND I would try different crystals to check their ability to start-up (and hold).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2012 23:40:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Vbat-RTC-problems/m-p/173866#M1360</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2012-07-17T23:40:51Z</dc:date>
    </item>
  </channel>
</rss>