<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Code Warrior Not Recognising CPU Registers in ISR in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-Warrior-Not-Recognising-CPU-Registers-in-ISR/m-p/312309#M13503</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am developing a HAL for a university project on the Kinetis K70 tower modue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Codewarrior 10.4 and have written the following ISR for the supervisor call to set the code to privelliged mode..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void isrSVCint(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t control;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t * controlPtr;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; control = 0x00000000;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; controlPtr = &amp;amp;control;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("LDR R1,[controlPtr,0]");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("MSR CONTROL, R1");&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The second ASM line is throwing an "unknown identifier: R1" error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The previous line accept R1 without issue, so I am wondering what is occuring here...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think I have probably missed something fairly basic here, Please advise...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ben&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Apr 2014 04:22:46 GMT</pubDate>
    <dc:creator>benjames</dc:creator>
    <dc:date>2014-04-08T04:22:46Z</dc:date>
    <item>
      <title>Code Warrior Not Recognising CPU Registers in ISR</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-Warrior-Not-Recognising-CPU-Registers-in-ISR/m-p/312309#M13503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am developing a HAL for a university project on the Kinetis K70 tower modue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Codewarrior 10.4 and have written the following ISR for the supervisor call to set the code to privelliged mode..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void isrSVCint(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t control;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t * controlPtr;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; control = 0x00000000;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; controlPtr = &amp;amp;control;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("LDR R1,[controlPtr,0]");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("MSR CONTROL, R1");&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The second ASM line is throwing an "unknown identifier: R1" error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The previous line accept R1 without issue, so I am wondering what is occuring here...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think I have probably missed something fairly basic here, Please advise...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ben&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Apr 2014 04:22:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-Warrior-Not-Recognising-CPU-Registers-in-ISR/m-p/312309#M13503</guid>
      <dc:creator>benjames</dc:creator>
      <dc:date>2014-04-08T04:22:46Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior Not Recognising CPU Registers in ISR</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-Warrior-Not-Recognising-CPU-Registers-in-ISR/m-p/312310#M13504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ben James,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think there is some asm syntax issue in your code, please kindly use the following code instead.&lt;/P&gt;&lt;P&gt;uint32_t control;&lt;/P&gt;&lt;P&gt;int main(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; int counter = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; control = 0x00000000;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("LDR R7,=control\n\t");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("MSR CONTROL, R7");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for(;;) {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; counter++;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return 0;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Apr 2014 06:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-Warrior-Not-Recognising-CPU-Registers-in-ISR/m-p/312310#M13504</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-04-09T06:49:55Z</dc:date>
    </item>
  </channel>
</rss>