<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックSimple UART on KL26Z</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Simple-UART-on-KL26Z/m-p/312293#M13501</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on an I2S application for my university although I need UART enabled for various development purposes.&lt;BR /&gt;I have worked with UART with AVR controllers although the application needs the higher powered 32-bit capabilities of the KL26Z&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my experience with AVRs, using the UART was simply setting simple parameters in the UART control registers and then enabling them and using simple functions.&lt;BR /&gt;Does anybody have code I could use or point me in the right direction?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Apr 2014 02:36:56 GMT</pubDate>
    <dc:creator>funkyguy4000</dc:creator>
    <dc:date>2014-04-08T02:36:56Z</dc:date>
    <item>
      <title>Simple UART on KL26Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Simple-UART-on-KL26Z/m-p/312293#M13501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on an I2S application for my university although I need UART enabled for various development purposes.&lt;BR /&gt;I have worked with UART with AVR controllers although the application needs the higher powered 32-bit capabilities of the KL26Z&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my experience with AVRs, using the UART was simply setting simple parameters in the UART control registers and then enabling them and using simple functions.&lt;BR /&gt;Does anybody have code I could use or point me in the right direction?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Apr 2014 02:36:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Simple-UART-on-KL26Z/m-p/312293#M13501</guid>
      <dc:creator>funkyguy4000</dc:creator>
      <dc:date>2014-04-08T02:36:56Z</dc:date>
    </item>
    <item>
      <title>Re: Simple UART on KL26Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Simple-UART-on-KL26Z/m-p/312294#M13502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Shannon&lt;/P&gt;&lt;P&gt;I2S and I2C are not the same serial communication function. &lt;/P&gt;&lt;P&gt;For KL26Z, you can use KL26 sample code from link &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL26Z&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL26Z&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;FRDM-KL26Z: Freescale Freedom Development Platform for Kinetis KL16 and KL26 MCUs (up to 128 KB Flash)&lt;/A&gt; &lt;/P&gt;&lt;P&gt;The sample code named "FRDM_KL26_SC". After you install it, you can find demo code in path ...\FRDM-KL26Z_SC\FRDM-KL26Z_SC_Rev_1.0\klxx-sc-baremetal\build\iar\FRDM_KL26ZDemo. UART setting function is in C file sysinit.c.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Apr 2014 06:06:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Simple-UART-on-KL26Z/m-p/312294#M13502</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2014-04-08T06:06:33Z</dc:date>
    </item>
  </channel>
</rss>