<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Help with KwikStik j-link flashing external device.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-with-KwikStik-j-link-flashing-external-device/m-p/173717#M1343</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok got the problem.. athought the kwikstick is the Version 4 it still can't program external devices with the switch off.. turning on worked here...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Oct 2011 23:59:53 GMT</pubDate>
    <dc:creator>luisf_rossi</dc:creator>
    <dc:date>2011-10-11T23:59:53Z</dc:date>
    <item>
      <title>Help with KwikStik j-link flashing external device.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-with-KwikStik-j-link-flashing-external-device/m-p/173716#M1342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, i am trying to use the KwikStik j-link to flash an external Kinetis. For some reason it is not working and CodeWarrior is retrieving a message saying it could not reset the Kinetis.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I even tryed to remove the kinetis on the KwikStik board but with no change.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Kinetis connections can be seen on the atachement. Thats just a piece of the board but related to kinetis there are just some extra decoupling network on other sheets.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The cable and pinheaders i am using are the sugested by the manual.&lt;/P&gt;&lt;P&gt;the j-link connector is pretty close to the kinetis..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help is appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Oct 2011 23:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-with-KwikStik-j-link-flashing-external-device/m-p/173716#M1342</guid>
      <dc:creator>luisf_rossi</dc:creator>
      <dc:date>2011-10-11T23:09:04Z</dc:date>
    </item>
    <item>
      <title>Re: Help with KwikStik j-link flashing external device.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-with-KwikStik-j-link-flashing-external-device/m-p/173717#M1343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok got the problem.. athought the kwikstick is the Version 4 it still can't program external devices with the switch off.. turning on worked here...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Oct 2011 23:59:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-with-KwikStik-j-link-flashing-external-device/m-p/173717#M1343</guid>
      <dc:creator>luisf_rossi</dc:creator>
      <dc:date>2011-10-11T23:59:53Z</dc:date>
    </item>
  </channel>
</rss>