<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K10 VREFH/VREFL Input Capacitance (ADC Problem) in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-VREFH-VREFL-Input-Capacitance-ADC-Problem/m-p/310120#M13324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone experienced a similar problem with ADC inputs on the K10?&amp;nbsp; The steady-state value in the center of the display is the voltage I'm trying to read.&amp;nbsp; The ADC is reporting the value at the bottom of the spikes - in this case ~79 mV too low.&amp;nbsp; Perhaps I need more capacitance at the input, or less capacitance on the VREFH/L pins?&amp;nbsp; Any advice will be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44345i8AE805D46F7D1924/image-size/large?v=v2&amp;amp;px=999" title="temp input.jpg" alt="temp input.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Jun 2014 13:19:52 GMT</pubDate>
    <dc:creator>ttocsmi</dc:creator>
    <dc:date>2014-06-02T13:19:52Z</dc:date>
    <item>
      <title>K10 VREFH/VREFL Input Capacitance (ADC Problem)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-VREFH-VREFL-Input-Capacitance-ADC-Problem/m-p/310120#M13324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone experienced a similar problem with ADC inputs on the K10?&amp;nbsp; The steady-state value in the center of the display is the voltage I'm trying to read.&amp;nbsp; The ADC is reporting the value at the bottom of the spikes - in this case ~79 mV too low.&amp;nbsp; Perhaps I need more capacitance at the input, or less capacitance on the VREFH/L pins?&amp;nbsp; Any advice will be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44345i8AE805D46F7D1924/image-size/large?v=v2&amp;amp;px=999" title="temp input.jpg" alt="temp input.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jun 2014 13:19:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-VREFH-VREFL-Input-Capacitance-ADC-Problem/m-p/310120#M13324</guid>
      <dc:creator>ttocsmi</dc:creator>
      <dc:date>2014-06-02T13:19:52Z</dc:date>
    </item>
    <item>
      <title>Re: K10 VREFH/VREFL Input Capacitance (ADC Problem)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-VREFH-VREFL-Input-Capacitance-ADC-Problem/m-p/310121#M13325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott,&lt;/P&gt;&lt;P&gt;I'd like to suggest that the Vrefh should be stable voltage as possible, and please refer to AN4373 which about how to get the best performance of ADC.&lt;/P&gt;&lt;P&gt;I've also included the application note with this reply and check it.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jun 2014 07:10:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-VREFH-VREFL-Input-Capacitance-ADC-Problem/m-p/310121#M13325</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-06-03T07:10:48Z</dc:date>
    </item>
  </channel>
</rss>