<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: LCD16x2 and GCC compiler</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD16x2-and-GCC-compiler/m-p/309043#M13220</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Jorge_Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's really useful links.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Minh.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Apr 2014 14:31:37 GMT</pubDate>
    <dc:creator>nguyennhatminh</dc:creator>
    <dc:date>2014-04-04T14:31:37Z</dc:date>
    <item>
      <title>LCD16x2 and GCC compiler</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD16x2-and-GCC-compiler/m-p/309039#M13216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm going to build a driver that control the LCD 16x2 so I have a question about&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GCC compiler on Codewarrior IDE for FreedomKinetis KL05Z.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when I code :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example: printf(" I love freescale")&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;does it call the function putch(char c) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Apr 2014 15:30:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD16x2-and-GCC-compiler/m-p/309039#M13216</guid>
      <dc:creator>nguyennhatminh</dc:creator>
      <dc:date>2014-04-02T15:30:28Z</dc:date>
    </item>
    <item>
      <title>Re: LCD16x2 and GCC compiler</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD16x2-and-GCC-compiler/m-p/309040#M13217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Minh&lt;/P&gt;&lt;P&gt;Function printf does not call such function putch(char C). I cannot find which MCU you used, but I think you can develop your project base on our "hello world" demo.Then you no need to care about printf function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Apr 2014 08:25:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD16x2-and-GCC-compiler/m-p/309040#M13217</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2014-04-04T08:25:22Z</dc:date>
    </item>
    <item>
      <title>Re: LCD16x2 and GCC compiler</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD16x2-and-GCC-compiler/m-p/309041#M13218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Zhe Tian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply, would you like show me where is " Hello World" demo ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Minh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Apr 2014 09:10:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD16x2-and-GCC-compiler/m-p/309041#M13218</guid>
      <dc:creator>nguyennhatminh</dc:creator>
      <dc:date>2014-04-04T09:10:35Z</dc:date>
    </item>
    <item>
      <title>Re: LCD16x2 and GCC compiler</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD16x2-and-GCC-compiler/m-p/309042#M13219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you already downloaded the "KL05_SC" package. The project is called "kl05_frdm_demo"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However I think you might find that example difficult to figure out how to use your LCD with prinft.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case you need to create your own level driver so that the last function called is your specific function for talking with the LCD. I recommend you to check the next tutorial by colleague Erich Styger:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2013/04/17/printf-with-the-frdm-kl25z-board-and-without-processor-expert/" title="http://mcuoneclipse.com/2013/04/17/printf-with-the-frdm-kl25z-board-and-without-processor-expert/"&gt;printf() with the FRDM-KL25Z Board and without Processor Expert | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will see that in the file ConsoleIO.c, in the function __write_console() you have a call to UART0_PDD_PutChar8(). Here you would put instead your LCD function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And also if you are willing to use Processor Expert, then there is a LCD component created also by Erich. Check this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2012/12/22/hd44780-2x16-character-display-for-kinetis-and-freedom-board/" title="http://mcuoneclipse.com/2012/12/22/hd44780-2x16-character-display-for-kinetis-and-freedom-board/"&gt;HD44780 2×16 Character Display for Kinetis and Freedom Board | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Apr 2014 13:56:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD16x2-and-GCC-compiler/m-p/309042#M13219</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-04-04T13:56:58Z</dc:date>
    </item>
    <item>
      <title>Re: LCD16x2 and GCC compiler</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD16x2-and-GCC-compiler/m-p/309043#M13220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Jorge_Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's really useful links.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Minh.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Apr 2014 14:31:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LCD16x2-and-GCC-compiler/m-p/309043#M13220</guid>
      <dc:creator>nguyennhatminh</dc:creator>
      <dc:date>2014-04-04T14:31:37Z</dc:date>
    </item>
  </channel>
</rss>