<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Cannot Connect to E02</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-Connect-to-E02/m-p/308306#M13177</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you checked that the PE connection properties are set to SWD mode rather than JTAG mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jul 2014 15:09:27 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-07-11T15:09:27Z</dc:date>
    <item>
      <title>Cannot Connect to E02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-Connect-to-E02/m-p/308304#M13175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am in urgent need of some advice.&amp;nbsp; I submitted a support request to Freescale, waited 2 days, got a couple of not very helpful emails, and then he disappeared again for 2 days.&amp;nbsp; I've also contacted my vendor for FAE support, but have not yet heard back.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A week ago I got a new PC board for a MKE02Z64VLC2 (32 pin LQFP).&amp;nbsp; I had been successfully working with a Freedom board with the same device, using the OpenSDA.&amp;nbsp; With the new board, I'm switching to the PE Multilink.&amp;nbsp; But I cannot connect with CodeWarrior to the new board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Multilink turns on the blue LED when I enumerate on USB, and the yellow LED when I apply power to my target.&amp;nbsp; This makes me believe at least that part of the link from CodeWarrior to the EO2 is working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have verified that power and ground are fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nearly every pin on the device is I/O and all the signals appear to be normal (except for below).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Without the Multilink attached, there is no oscillation on the crystal.&amp;nbsp; I believe this is because it is not turned on in the completely blank new E02.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With or without the Multilink, there is a periodic sawtooth on /RESET.&amp;nbsp; The period is about 300 usec, or about 3K Hz.&amp;nbsp; I'm not sure, but I believe this might be the internal watchdog, also configured for default, to trigger at that period.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried the Kinetis recovery tool (with the Multilink, of course) many, many times, but it will not connect to the E02.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The weird symptoms are the CLK and DIO pins on the board are not normal.&amp;nbsp; I've looked at them with a 'scope while trying to connect with CodeWarrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CLK actually goes negative by about a volt.&amp;nbsp; First, there are no negative supplies on the board.&amp;nbsp; There are a couple of RS-232 drivers with internal negative voltages, but I've verified there are no shorts.&amp;nbsp; I've also verified there are no floating Vdd or GND pins on the E02 and SWD connector that would cause this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The DIO pin is also weird.&amp;nbsp; It sits somewhere between 4V and 5V, then starts toggling but not all the way between the rails.&amp;nbsp; And the high level seems to decay to a lower voltage with time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll attach some 'scope traces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the time reading my post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 May 2014 16:20:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-Connect-to-E02/m-p/308304#M13175</guid>
      <dc:creator>d_</dc:creator>
      <dc:date>2014-05-29T16:20:40Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot Connect to E02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-Connect-to-E02/m-p/308305#M13176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dave, I have the same question today.&amp;nbsp; Have you been able to connect the P&amp;amp;E Mulilink Universal to the KE02 microcontroller yet? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jul 2014 13:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-Connect-to-E02/m-p/308305#M13176</guid>
      <dc:creator>Kratz</dc:creator>
      <dc:date>2014-07-11T13:47:52Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot Connect to E02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-Connect-to-E02/m-p/308306#M13177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you checked that the PE connection properties are set to SWD mode rather than JTAG mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jul 2014 15:09:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-Connect-to-E02/m-p/308306#M13177</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-07-11T15:09:27Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot Connect to E02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-Connect-to-E02/m-p/308307#M13178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kevin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I found my problem.&amp;nbsp; Even though the schematic was correct, the library part for the header was a mirror image.&amp;nbsp; I didn't do the hardware on this board, but from now on I'll make sure to double check the layout guy.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have any other questions, feel free to post or send a PM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jul 2014 15:18:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-Connect-to-E02/m-p/308307#M13178</guid>
      <dc:creator>d_</dc:creator>
      <dc:date>2014-07-11T15:18:12Z</dc:date>
    </item>
  </channel>
</rss>