<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックHow to erase the FLBPR setting in K60?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-erase-the-FLBPR-setting-in-K60/m-p/305718#M12970</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use AN2295 bootloader on MK60FN1M0VLQ12. When I use the bootloader code, I make a mistake to enable "BOOTLOADER_FLASH_PROTECTION = 1" and I load this bootloader code into K60. &lt;/P&gt;&lt;P&gt;I think it enable FLBPR. When I try to disable "BOOTLOADER_FLASH_PROTECTION ", the IAR can't load&lt;/P&gt;&lt;P&gt;the new compiled code &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;into K60. There is only bootloader code without user application code in K60.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;How do I erase the FLBPR to load the new bootloader code and user application code?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 May 2014 01:58:37 GMT</pubDate>
    <dc:creator>kkkk</dc:creator>
    <dc:date>2014-05-27T01:58:37Z</dc:date>
    <item>
      <title>How to erase the FLBPR setting in K60?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-erase-the-FLBPR-setting-in-K60/m-p/305718#M12970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use AN2295 bootloader on MK60FN1M0VLQ12. When I use the bootloader code, I make a mistake to enable "BOOTLOADER_FLASH_PROTECTION = 1" and I load this bootloader code into K60. &lt;/P&gt;&lt;P&gt;I think it enable FLBPR. When I try to disable "BOOTLOADER_FLASH_PROTECTION ", the IAR can't load&lt;/P&gt;&lt;P&gt;the new compiled code &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;into K60. There is only bootloader code without user application code in K60.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;How do I erase the FLBPR to load the new bootloader code and user application code?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 May 2014 01:58:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-erase-the-FLBPR-setting-in-K60/m-p/305718#M12970</guid>
      <dc:creator>kkkk</dc:creator>
      <dc:date>2014-05-27T01:58:37Z</dc:date>
    </item>
    <item>
      <title>Re: How to erase the FLBPR setting in K60?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-erase-the-FLBPR-setting-in-K60/m-p/305719#M12971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The "BOOTLOADER_FLASH_PROTECTION = 1" will protect bootloader ROM with modify Flash configuration field addrss 0x408~0x40B values.&lt;/P&gt;&lt;P&gt;Customer can use JTAG debugger tool do mass erase to remove Flash configuration field Flash protection value, even though Flash configuration field address is protected.&lt;/P&gt;&lt;P&gt;Such as using Segger J-Link tool, at J-Link Commander tool to run "unlock Kinetis" command.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 May 2014 04:01:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-erase-the-FLBPR-setting-in-K60/m-p/305719#M12971</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-05-29T04:01:28Z</dc:date>
    </item>
    <item>
      <title>Re: How to erase the FLBPR setting in K60?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-erase-the-FLBPR-setting-in-K60/m-p/305720#M12972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It works. Thanks a lot for help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jun 2014 02:34:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-erase-the-FLBPR-setting-in-K60/m-p/305720#M12972</guid>
      <dc:creator>kkkk</dc:creator>
      <dc:date>2014-06-03T02:34:55Z</dc:date>
    </item>
  </channel>
</rss>