<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FAT32 File System with SPI Flash</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FAT32-File-System-with-SPI-Flash/m-p/305257#M12943</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to implement the file system in SPI Flash?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 May 2014 12:00:40 GMT</pubDate>
    <dc:creator>yasararafathcs</dc:creator>
    <dc:date>2014-05-27T12:00:40Z</dc:date>
    <item>
      <title>FAT32 File System with SPI Flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FAT32-File-System-with-SPI-Flash/m-p/305254#M12940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on Kinetis KL46 processor with SPI Flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am in need of implemented SPI Flash drivers for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will anyone can provide me please?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanking you,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 May 2014 12:20:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FAT32-File-System-with-SPI-Flash/m-p/305254#M12940</guid>
      <dc:creator>yasararafathcs</dc:creator>
      <dc:date>2014-05-26T12:20:59Z</dc:date>
    </item>
    <item>
      <title>Re: FAT32 File System with SPI Flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FAT32-File-System-with-SPI-Flash/m-p/305255#M12941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the KL46 source code you can find an example which uses the SPI module with the DMA feature. There you can find drivers for the SPI module&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KL46 Source Code:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL46Z&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL46Z&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;FRDM-KL46Z: Freescale Freedom Development Platform for Kinetis KL3x and KL4x MCUs&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you do not want to download the complete package in the attachments you can find the source code of this project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. It would be nice!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 May 2014 16:13:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FAT32-File-System-with-SPI-Flash/m-p/305255#M12941</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2014-05-26T16:13:21Z</dc:date>
    </item>
    <item>
      <title>Re: FAT32 File System with SPI Flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FAT32-File-System-with-SPI-Flash/m-p/305256#M12942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KL46 is supported in the uTasker project (TWR-KL46 and FRDM-KL46 as immediate target builds) with utFAT on SD cards via the SPI (or uFileSystem in ATMEL 45DB xxx, SST25xxx or ST 25Pxxx serial flash). See below simulations of the two boards operating with SD card and driving SLCDs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44062i14196C7073018B21/image-size/large?v=v2&amp;amp;px=999" title="twr-kl46.png" alt="twr-kl46.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44117iC5057B66003344DE/image-size/large?v=v2&amp;amp;px=999" title="frd-kl46.png" alt="frd-kl46.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 May 2014 21:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FAT32-File-System-with-SPI-Flash/m-p/305256#M12942</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-05-26T21:52:06Z</dc:date>
    </item>
    <item>
      <title>Re: FAT32 File System with SPI Flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FAT32-File-System-with-SPI-Flash/m-p/305257#M12943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to implement the file system in SPI Flash?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 May 2014 12:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FAT32-File-System-with-SPI-Flash/m-p/305257#M12943</guid>
      <dc:creator>yasararafathcs</dc:creator>
      <dc:date>2014-05-27T12:00:40Z</dc:date>
    </item>
  </channel>
</rss>