<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: How to Make DMA-UART work with KL05 and series?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Make-DMA-UART-work-with-KL05-and-series/m-p/304247#M12870</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Amit,&lt;/P&gt;&lt;P&gt;I'd like to suggest that you can refer to low_power_dma_uart_demo in KL25 sample code.&lt;/P&gt;&lt;P&gt;The demo is about UART work with DMA.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 May 2014 01:57:40 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2014-05-28T01:57:40Z</dc:date>
    <item>
      <title>How to Make DMA-UART work with KL05 and series?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Make-DMA-UART-work-with-KL05-and-series/m-p/304246#M12869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using code warrior 10.5 along with PE , I wanted to test a program in which I will be sending some commands using terminal window to UART0 and it will be received through DMA and will send it back to the terminal(with or without DMA). I have done this for K20 and other K series and it is working fine. But it didn't work with Kl05 and FRDM-Kl46Z here is the attached code . I tried the sample code present in the codewarrior for MKL05Z32VLF4. and also tried the code given in &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fquick_ref_guide%2FKLQRUG.pdf%3Ffpsp%3D1%26WT_TYPE%3DUsers%2520Guides%26WT_VENDOR%3DFREESCALE%26WT_FILE_FORMAT%3Dpdf%26WT_ASSET%3DDocumentation" rel="nofollow" target="_blank"&gt;KLQRG&lt;/A&gt;, chapter no 7. even that didn't work. Please look into the matter and resolve this issue.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Amit Kumar&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337564"&gt;kl05-DMA-testing-23-05-2014.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 May 2014 13:10:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Make-DMA-UART-work-with-KL05-and-series/m-p/304246#M12869</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2014-05-23T13:10:47Z</dc:date>
    </item>
    <item>
      <title>Re: How to Make DMA-UART work with KL05 and series?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Make-DMA-UART-work-with-KL05-and-series/m-p/304247#M12870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Amit,&lt;/P&gt;&lt;P&gt;I'd like to suggest that you can refer to low_power_dma_uart_demo in KL25 sample code.&lt;/P&gt;&lt;P&gt;The demo is about UART work with DMA.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 May 2014 01:57:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Make-DMA-UART-work-with-KL05-and-series/m-p/304247#M12870</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-05-28T01:57:40Z</dc:date>
    </item>
  </channel>
</rss>