<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: voltage input range of Kinetis M ADC in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/voltage-input-range-of-Kinetis-M-ADC/m-p/303470#M12816</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Without being familiar with the KM34 in question, I will just state that by definition a differential input to an ADC is 'oblivious' to the common-mode voltage on the signal pair -- this is 'subtracted' directly by a front-end differential amplifier -- so in your case, put your positive signal on the '+' input, and put VCC-to-the-module/2 to the '-' input to properly subtract the chip's DC offset.&amp;nbsp; What you DO need to know in that regard is the allowed signal-range for said diff-amp.&amp;nbsp; If the inputs are 'fully operational' over the 2 to 3V range, then you will properly net +/-400mV into the ADC directly from your sensor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some further investigation into the matter indicates you are looking at the sigma-delta ADC, and the common-mode voltage spec there is 0 to 0.8V -- so too low for my 'direct connection' assumption (which was more based on the differential functions available in some other Kinetis parts to the SAR ADC).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 May 2014 14:19:13 GMT</pubDate>
    <dc:creator>egoodii</dc:creator>
    <dc:date>2014-05-23T14:19:13Z</dc:date>
    <item>
      <title>voltage input range of Kinetis M ADC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/voltage-input-range-of-Kinetis-M-ADC/m-p/303469#M12815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i want to use a Halleffect sensor(&lt;A href="http://www.robotshop.com/en/pololu-30a-acs714-current-sensor.html" title="http://www.robotshop.com/en/pololu-30a-acs714-current-sensor.html"&gt;Pololu ±30A ACS714 Current Sensor - RobotShop&lt;/A&gt;) in combination with the TWR-KM34(Kinetis M3). According to the Ddatasheet the differential inputs accept a voltage range of 1V (+-500mV).&lt;/P&gt;&lt;P&gt;But the sensor exclusively has positive output: centered at 2,5V +-400mV&lt;/P&gt;&lt;P&gt;Does the firmware of TWR-KM34 properly work if my input signal is 0 to +500mV(so i could simply use a voltage divider)?&lt;/P&gt;&lt;P&gt;Or is it possible to change the input rane of hte ADCs from +-500mV to 2V+-500mV?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 May 2014 13:46:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/voltage-input-range-of-Kinetis-M-ADC/m-p/303469#M12815</guid>
      <dc:creator>svenmoeller</dc:creator>
      <dc:date>2014-05-22T13:46:20Z</dc:date>
    </item>
    <item>
      <title>Re: voltage input range of Kinetis M ADC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/voltage-input-range-of-Kinetis-M-ADC/m-p/303470#M12816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Without being familiar with the KM34 in question, I will just state that by definition a differential input to an ADC is 'oblivious' to the common-mode voltage on the signal pair -- this is 'subtracted' directly by a front-end differential amplifier -- so in your case, put your positive signal on the '+' input, and put VCC-to-the-module/2 to the '-' input to properly subtract the chip's DC offset.&amp;nbsp; What you DO need to know in that regard is the allowed signal-range for said diff-amp.&amp;nbsp; If the inputs are 'fully operational' over the 2 to 3V range, then you will properly net +/-400mV into the ADC directly from your sensor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some further investigation into the matter indicates you are looking at the sigma-delta ADC, and the common-mode voltage spec there is 0 to 0.8V -- so too low for my 'direct connection' assumption (which was more based on the differential functions available in some other Kinetis parts to the SAR ADC).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 May 2014 14:19:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/voltage-input-range-of-Kinetis-M-ADC/m-p/303470#M12816</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2014-05-23T14:19:13Z</dc:date>
    </item>
  </channel>
</rss>