<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックUpdated Project for USB Host Stack v4.1.1 msd_mfs_generic kinetis_l2k</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Updated-Project-for-USB-Host-Stack-v4-1-1-msd-mfs-generic/m-p/301787#M12682</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was working with the latest MCU Baremetal USB stack v4.1.1, trying to build the example project for the msd_mfs_generic on the Kinetis L KL25.&amp;nbsp; This example uses the USB Host stack to mount a USB flash drive.&amp;nbsp; The projects for the KL25 are called kinetis_l2k.&amp;nbsp; But I found that the CodeWarrior project for this example would not build in CodeWarrior v10.6.&amp;nbsp; I had to modify the project, and one source file to get it to build, and attached is the patch to use with these changes.&amp;nbsp; I tested this with the Tower board TWR-KL25Z48M.&amp;nbsp; Also note, this example uses UART0 on the KL25 to print to the terminal.&amp;nbsp; This does not go to the OpenSDA COM port, or the TWR-SER serial port.&amp;nbsp; Instead, the UART Tx signal goes to signal A42 of the Tower edge connector.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To apply this patch, unzip the attached file with the CodeWarrior project closed to the directory \Freescale USB Stack v4.1.1\Source\Host\examples\msd_mfs_generic, then import the project directory into CodeWarrior C:\Freescale\Freescale USB Stack v4.1.1\Source\Host\examples\msd_mfs_generic\cw10\kinetis_l2k&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337678"&gt;msd_mfs_generic_kinetis_l2k.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 May 2014 14:47:45 GMT</pubDate>
    <dc:creator>dereksnell</dc:creator>
    <dc:date>2014-05-20T14:47:45Z</dc:date>
    <item>
      <title>Updated Project for USB Host Stack v4.1.1 msd_mfs_generic kinetis_l2k</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Updated-Project-for-USB-Host-Stack-v4-1-1-msd-mfs-generic/m-p/301787#M12682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was working with the latest MCU Baremetal USB stack v4.1.1, trying to build the example project for the msd_mfs_generic on the Kinetis L KL25.&amp;nbsp; This example uses the USB Host stack to mount a USB flash drive.&amp;nbsp; The projects for the KL25 are called kinetis_l2k.&amp;nbsp; But I found that the CodeWarrior project for this example would not build in CodeWarrior v10.6.&amp;nbsp; I had to modify the project, and one source file to get it to build, and attached is the patch to use with these changes.&amp;nbsp; I tested this with the Tower board TWR-KL25Z48M.&amp;nbsp; Also note, this example uses UART0 on the KL25 to print to the terminal.&amp;nbsp; This does not go to the OpenSDA COM port, or the TWR-SER serial port.&amp;nbsp; Instead, the UART Tx signal goes to signal A42 of the Tower edge connector.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To apply this patch, unzip the attached file with the CodeWarrior project closed to the directory \Freescale USB Stack v4.1.1\Source\Host\examples\msd_mfs_generic, then import the project directory into CodeWarrior C:\Freescale\Freescale USB Stack v4.1.1\Source\Host\examples\msd_mfs_generic\cw10\kinetis_l2k&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337678"&gt;msd_mfs_generic_kinetis_l2k.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 May 2014 14:47:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Updated-Project-for-USB-Host-Stack-v4-1-1-msd-mfs-generic/m-p/301787#M12682</guid>
      <dc:creator>dereksnell</dc:creator>
      <dc:date>2014-05-20T14:47:45Z</dc:date>
    </item>
  </channel>
</rss>