<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 FRDM-KE02Z with an external SWD programmer/debugger</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KE02Z-with-an-external-SWD-programmer-debugger/m-p/300083#M12496</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a Kinetis E series evaluation board, the FRDM-KE02Z, and also have a USBDM that supports programming the MKE02Z64 (MKE02Z64VQH2) chip present on this board. I am interested in using this external programmer instead of the onboard OpenSDA programmer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I removed the 0 ohm resistor R35 and populated J5 with a header so I can put a jumper block on it. When the jumper is not present, the target chip's reset line is isolated from OpenSDA output for it. The other clock and data lines involved with SWD aren't isolated technically, but there are tri-state buffers that the OpenSDA chip usually leaves disconnected unless it's trying to program the target (I assume.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when I try flashing an empty barebones project in CodeWarrior using the USBDM I get an error:&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;Error launching testprj_FLASH_USBDM&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;ARM GDI Protocol Adapter : Can't connect. BDM has no connection to target&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I don't have the development board's mini-USB connector attached to my computer providing power to the board, I get this error message instead:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;Error launching testprj_FLASH_USBDM&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;ARM GDI Protocol Adapter : Can't connect. Target Vdd not present&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This leads me to believe that the USBDM is working as far as it's ability to detect Vdd (aka Vcc), but can't actually communicate with the target chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone used an external programmer with the FRDM-KE02Z? If so, what's the trick to it? I'd especially like to know if anyone's done it with the USBDM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 18 May 2014 10:47:35 GMT</pubDate>
    <dc:creator>fdarling</dc:creator>
    <dc:date>2014-05-18T10:47:35Z</dc:date>
    <item>
      <title>FRDM-KE02Z with an external SWD programmer/debugger</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KE02Z-with-an-external-SWD-programmer-debugger/m-p/300083#M12496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a Kinetis E series evaluation board, the FRDM-KE02Z, and also have a USBDM that supports programming the MKE02Z64 (MKE02Z64VQH2) chip present on this board. I am interested in using this external programmer instead of the onboard OpenSDA programmer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I removed the 0 ohm resistor R35 and populated J5 with a header so I can put a jumper block on it. When the jumper is not present, the target chip's reset line is isolated from OpenSDA output for it. The other clock and data lines involved with SWD aren't isolated technically, but there are tri-state buffers that the OpenSDA chip usually leaves disconnected unless it's trying to program the target (I assume.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when I try flashing an empty barebones project in CodeWarrior using the USBDM I get an error:&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;Error launching testprj_FLASH_USBDM&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;ARM GDI Protocol Adapter : Can't connect. BDM has no connection to target&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I don't have the development board's mini-USB connector attached to my computer providing power to the board, I get this error message instead:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;Error launching testprj_FLASH_USBDM&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;ARM GDI Protocol Adapter : Can't connect. Target Vdd not present&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This leads me to believe that the USBDM is working as far as it's ability to detect Vdd (aka Vcc), but can't actually communicate with the target chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone used an external programmer with the FRDM-KE02Z? If so, what's the trick to it? I'd especially like to know if anyone's done it with the USBDM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 May 2014 10:47:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KE02Z-with-an-external-SWD-programmer-debugger/m-p/300083#M12496</guid>
      <dc:creator>fdarling</dc:creator>
      <dc:date>2014-05-18T10:47:35Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KE02Z with an external SWD programmer/debugger</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KE02Z-with-an-external-SWD-programmer-debugger/m-p/300084#M12497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not sure if the USBDM requires the reset line, but I would keep J5 placed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I think there are different versions of USBDM hardware, some seem to use JTAG and some others SWD, and FRDM-KE02 requires SWD. Have you verified that your hardware can program through SWD?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our colleague Erich Styger ran into a similar problem like yours and he tried some alternatives. Check the next thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2013/05/09/usbdm-4-10-5-supports-now-mcu10-4/" title="http://mcuoneclipse.com/2013/05/09/usbdm-4-10-5-supports-now-mcu10-4/"&gt;USBDM 4.10.5 supports now MCU10.4 | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;User &lt;STRONG&gt;pgo&lt;/STRONG&gt; is the developer of USBDM and he could provide a better insight in this. A problem with KE02 was reported already, maybe you can ask him in that thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/323669"&gt;it is failed to program application into MKE02Z64&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope some of this helps!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 May 2014 14:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KE02Z-with-an-external-SWD-programmer-debugger/m-p/300084#M12497</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-05-22T14:16:01Z</dc:date>
    </item>
  </channel>
</rss>