<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KwikStik UART with tower TWR-SER</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-UART-with-tower-TWR-SER/m-p/172058#M1245</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem seems to be with my USB-serial adapter. &amp;nbsp;It is working now.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The next issue is that I cannot connect to the kwikstik with J-link when it is plugged into the tower unit. Is there any way to do this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jun 2012 06:41:59 GMT</pubDate>
    <dc:creator>dan_quist</dc:creator>
    <dc:date>2012-06-14T06:41:59Z</dc:date>
    <item>
      <title>KwikStik UART with tower TWR-SER</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-UART-with-tower-TWR-SER/m-p/172057#M1244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to use the tower TWR-SER module with the KwikStik to route UART data to my PC. I can probe the UART5 test point on the kwikstik board and see the data, but I can't get anything out of the serial module. I have all the jumpers set to RS-232. Is there something special I need to do to get this to work?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jun 2012 05:04:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-UART-with-tower-TWR-SER/m-p/172057#M1244</guid>
      <dc:creator>dan_quist</dc:creator>
      <dc:date>2012-06-14T05:04:19Z</dc:date>
    </item>
    <item>
      <title>Re: KwikStik UART with tower TWR-SER</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-UART-with-tower-TWR-SER/m-p/172058#M1245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem seems to be with my USB-serial adapter. &amp;nbsp;It is working now.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The next issue is that I cannot connect to the kwikstik with J-link when it is plugged into the tower unit. Is there any way to do this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jun 2012 06:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-UART-with-tower-TWR-SER/m-p/172058#M1245</guid>
      <dc:creator>dan_quist</dc:creator>
      <dc:date>2012-06-14T06:41:59Z</dc:date>
    </item>
    <item>
      <title>Re: KwikStik UART with tower TWR-SER</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-UART-with-tower-TWR-SER/m-p/172059#M1246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you haven't sorted your problem already...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think you need to connect one USB cable to provide power to the TOWER. You need a second USB link via the J-Link. IIRC you need to tell the IDE which debugger you are using.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Good luck.&lt;/P&gt;&lt;P&gt;Smiler.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2012 14:40:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-UART-with-tower-TWR-SER/m-p/172059#M1246</guid>
      <dc:creator>Smiler</dc:creator>
      <dc:date>2012-07-23T14:40:50Z</dc:date>
    </item>
    <item>
      <title>Re: KwikStik UART with tower TWR-SER</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-UART-with-tower-TWR-SER/m-p/172060#M1247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your reply, but that doesn't address the issue of the A/D not working. I am trying to run the adc example for twrk53 without any changes and it does 3 or 4 conversions and then just stops working.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Jul 2012 04:41:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KwikStik-UART-with-tower-TWR-SER/m-p/172060#M1247</guid>
      <dc:creator>dan_quist</dc:creator>
      <dc:date>2012-07-28T04:41:12Z</dc:date>
    </item>
  </channel>
</rss>