<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックHelp with a FRDM-KL25Z file download problem?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-with-a-FRDM-KL25Z-file-download-problem/m-p/299519#M12447</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having trouble copying files to my FRDM-KL25Z boards. When it works a dialog box briefly appears saying "Copying 1 item" and the transfer is successful and the program starts running. In the failure mode the dialog box does not appear, the file name appears instantly in the FRDM-KL25Z Windows Explorer window, and the small LED associated with the OpenSDA interface flashes quickly - 7 or 8 flashes and a pause - repeatedly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This behaviour is intermittent. I cannot see a pattern. I get the same result with several FRDM boards, with two laptops (both Windows 7). I have the latest PE Micro OpenSDA firmware loaded and the latest USB drivers on both machines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe the FRDM-KL25Z hardware is working as (a) the boards always enumerate as FRDM-KL25Z disk drives, (b) I have no trouble updating OpenSDA firmware and (c) even if the download fails the previously loaded KL25Z &lt;/P&gt;&lt;P&gt;firmware continues to run.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It feels like a device driver fault or a USB fault, or perhaps a fault with the connection between the two processors on the FRDM board. Has anyone else seen this problem? How do I fix it? Help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Mar 2014 13:59:07 GMT</pubDate>
    <dc:creator>charlespalmer</dc:creator>
    <dc:date>2014-03-19T13:59:07Z</dc:date>
    <item>
      <title>Help with a FRDM-KL25Z file download problem?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-with-a-FRDM-KL25Z-file-download-problem/m-p/299519#M12447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having trouble copying files to my FRDM-KL25Z boards. When it works a dialog box briefly appears saying "Copying 1 item" and the transfer is successful and the program starts running. In the failure mode the dialog box does not appear, the file name appears instantly in the FRDM-KL25Z Windows Explorer window, and the small LED associated with the OpenSDA interface flashes quickly - 7 or 8 flashes and a pause - repeatedly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This behaviour is intermittent. I cannot see a pattern. I get the same result with several FRDM boards, with two laptops (both Windows 7). I have the latest PE Micro OpenSDA firmware loaded and the latest USB drivers on both machines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe the FRDM-KL25Z hardware is working as (a) the boards always enumerate as FRDM-KL25Z disk drives, (b) I have no trouble updating OpenSDA firmware and (c) even if the download fails the previously loaded KL25Z &lt;/P&gt;&lt;P&gt;firmware continues to run.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It feels like a device driver fault or a USB fault, or perhaps a fault with the connection between the two processors on the FRDM board. Has anyone else seen this problem? How do I fix it? Help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Mar 2014 13:59:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-with-a-FRDM-KL25Z-file-download-problem/m-p/299519#M12447</guid>
      <dc:creator>charlespalmer</dc:creator>
      <dc:date>2014-03-19T13:59:07Z</dc:date>
    </item>
    <item>
      <title>Re: Help with a FRDM-KL25Z file download problem?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-with-a-FRDM-KL25Z-file-download-problem/m-p/299520#M12448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;it could be multiple reasons, the ones I have seen the most are:&lt;/P&gt;&lt;P&gt;- Win 8.x (but you say you are using Win7, so this should be fine)&lt;/P&gt;&lt;P&gt;- virus scanner&lt;/P&gt;&lt;P&gt;- using of a file commander/accelerator ==&amp;gt; use the DOS shell copy command instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;see &lt;A href="http://mcuoneclipse.com/2013/10/07/frdm-boards-not-responding-check-your-virus-scanner/" title="http://mcuoneclipse.com/2013/10/07/frdm-boards-not-responding-check-your-virus-scanner/"&gt;FRDM Board not responding? Check your Virus Scanner! | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Mar 2014 14:04:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-with-a-FRDM-KL25Z-file-download-problem/m-p/299520#M12448</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-03-19T14:04:37Z</dc:date>
    </item>
  </channel>
</rss>