<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: flexram to  eep in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexram-to-eep/m-p/299379#M12439</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 何胜利，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please kindly refer to the following answer for your question:&lt;/P&gt;&lt;P&gt;1，what is D-FLAS 0 IFR abs address ?&amp;nbsp; CAN I read it from IAR debug?&lt;/P&gt;&lt;P&gt;-D-FLAS 0 IFR can only be accessed by Read Resource Command, please refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44309iA67ED54154EF2180/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2，How many bytes about 1 Flash Block,1&amp;nbsp; Flash Section,where to set it?&lt;/P&gt;&lt;P&gt;-Do you mean flash section instead of flash section? Actually the size of flash block and sector are determined by device, no register can be used to configure them on the fly. Please kindly refer to Chapter 3 Chip Configuration in RM for details. You may find something like below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44352i6DE9F9BD1EC44B7E/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3,when I earse one&amp;nbsp; Flash Section ,how many byte I earsed ? earsing&amp;nbsp; start address is setted by FTFE_FCCOB1,FTFE_FCCOB2,FTFE_FCCOB3?&lt;/P&gt;&lt;P&gt;-Do you mean erasing Flash sector command? Then the bytes to be erased is size of a sector, for example, 4KB. and yes, earsing&amp;nbsp; start address is setted by FTFE_FCCOB1,FTFE_FCCOB2,FTFE_FCCOB3. Please refer to the following for more details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41370iB5C76F9E217051FB/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Apr 2014 08:56:32 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2014-04-21T08:56:32Z</dc:date>
    <item>
      <title>flexram to  eep</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexram-to-eep/m-p/299378#M12438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use flexram to eep! &lt;/P&gt;&lt;P&gt;MY CPU IS MK60FX512VLQ15,&lt;/P&gt;&lt;P&gt;1，what is D-FLAS 0 IFR abs address ?&amp;nbsp; CAN I read it from IAR debug?&lt;/P&gt;&lt;P&gt;2，How many bytes about 1 Flash Block,1&amp;nbsp; Flash Section,where to set it?&lt;/P&gt;&lt;P&gt;3,when I earse one&amp;nbsp; Flash Section ,how many byte I earsed ? earsing&amp;nbsp; start address is setted by FTFE_FCCOB1,FTFE_FCCOB2,FTFE_FCCOB3?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Apr 2014 01:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexram-to-eep/m-p/299378#M12438</guid>
      <dc:creator>胜利何</dc:creator>
      <dc:date>2014-04-18T01:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: flexram to  eep</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexram-to-eep/m-p/299379#M12439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 何胜利，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please kindly refer to the following answer for your question:&lt;/P&gt;&lt;P&gt;1，what is D-FLAS 0 IFR abs address ?&amp;nbsp; CAN I read it from IAR debug?&lt;/P&gt;&lt;P&gt;-D-FLAS 0 IFR can only be accessed by Read Resource Command, please refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44309iA67ED54154EF2180/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2，How many bytes about 1 Flash Block,1&amp;nbsp; Flash Section,where to set it?&lt;/P&gt;&lt;P&gt;-Do you mean flash section instead of flash section? Actually the size of flash block and sector are determined by device, no register can be used to configure them on the fly. Please kindly refer to Chapter 3 Chip Configuration in RM for details. You may find something like below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44352i6DE9F9BD1EC44B7E/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3,when I earse one&amp;nbsp; Flash Section ,how many byte I earsed ? earsing&amp;nbsp; start address is setted by FTFE_FCCOB1,FTFE_FCCOB2,FTFE_FCCOB3?&lt;/P&gt;&lt;P&gt;-Do you mean erasing Flash sector command? Then the bytes to be erased is size of a sector, for example, 4KB. and yes, earsing&amp;nbsp; start address is setted by FTFE_FCCOB1,FTFE_FCCOB2,FTFE_FCCOB3. Please refer to the following for more details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41370iB5C76F9E217051FB/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Apr 2014 08:56:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexram-to-eep/m-p/299379#M12439</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-04-21T08:56:32Z</dc:date>
    </item>
  </channel>
</rss>