<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 VREFH and VREFL connections for K60 when not using ADC</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VREFH-and-VREFL-connections-for-K60-when-not-using-ADC/m-p/298388#M12349</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to determine if I can tie my VREFH and VREFL lines directly to digital ground if I am not using the ADC of the K60.&amp;nbsp; I of course would keep VDDA connected to VDD, and put a decoupling cap on VREF_OUT, but wondering if I need to decouple VREFH and VREFL if I am not using them.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Mar 2014 14:28:09 GMT</pubDate>
    <dc:creator>tommyb</dc:creator>
    <dc:date>2014-03-18T14:28:09Z</dc:date>
    <item>
      <title>VREFH and VREFL connections for K60 when not using ADC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VREFH-and-VREFL-connections-for-K60-when-not-using-ADC/m-p/298388#M12349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to determine if I can tie my VREFH and VREFL lines directly to digital ground if I am not using the ADC of the K60.&amp;nbsp; I of course would keep VDDA connected to VDD, and put a decoupling cap on VREF_OUT, but wondering if I need to decouple VREFH and VREFL if I am not using them.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Mar 2014 14:28:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VREFH-and-VREFL-connections-for-K60-when-not-using-ADC/m-p/298388#M12349</guid>
      <dc:creator>tommyb</dc:creator>
      <dc:date>2014-03-18T14:28:09Z</dc:date>
    </item>
    <item>
      <title>Re: VREFH and VREFL connections for K60 when not using ADC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VREFH-and-VREFL-connections-for-K60-when-not-using-ADC/m-p/298389#M12350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tommy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The recommendation is to connect VREFH to VDD and VREFL to GND. This helps with the noise immunity.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Mar 2014 04:39:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VREFH-and-VREFL-connections-for-K60-when-not-using-ADC/m-p/298389#M12350</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-03-19T04:39:14Z</dc:date>
    </item>
  </channel>
</rss>